Skip to main content
SDall
Associate III
Feb 18, 2021 11:38 AM UTC
Question

problem to write to sdcard with f 401

hi i have a problem with sd card, i am trying to write a file.txt using the fats library

i am using cube mx old version and sdio reader data0, clk, cmd ....

here the code:

 MX_GPIO_Init ();

 MX_USART2_UART_Init ();

 MX_SDIO_SD_Init ();

 MX_FATFS_Init ();

 / * USER CODE BEGIN 2 * /

 / * USER CODE END 2 * /

 UINT testbyte;

  / * USER CODE BEGIN 2 * /

  FATFS myFATFS;

  FIL myFILE;

  if (f_mount (& myFATFS, SDPath, 1) == FR_OK) {

  HAL_GPIO_TogglePin (LD2_GPIO_Port, LD2_Pin);

  char mypath [] = "test1.txt";

  char myData [] = "hello world";

  if (f_open (& myFILE, mypath, FA_WRITE | FA_CREATE_ALWAYS) == FR_OK) {

  HAL_GPIO_TogglePin (LD2_GPIO_Port, LD2_Pin);

  if (fwrite (& myFILE, myData, sizeof (myData), & testbyte) == FR_OK) {

  HAL_GPIO_TogglePin (LD2_GPIO_Port, LD2_Pin);

  }

  f_close (& myFILE);

  }

the problem that enters f_mount, opens the file then f_write is ok but when I go to check the sd card I see the file open but no data written ...

thank you

This topic has been closed for replies.

1 reply

SDall
SDallAuthor
Associate III
Feb 18, 2021 11:39 AM UTC

i use sd card 4bit no dma