Skip to main content
Associate
October 26, 2025
Question

Problem in NetXDuo when selecting RGMII mode in ETH1

I am trying to do tcp client application with stm32n6570-dk board and when  I select RGMII mode in ETH1, ethernet interface is grayed out in network interface settings in netxduo. How can I fix it?

Cube IDE versiyon is 1.19.0, CubeMX version is 6.15.0 -RC7.

6 replies

Issamos
Super User
October 26, 2025

Hello @erik71 

I suggest you to put the cursor on the greyed option (ethernet interface under network interface settings in netxduo). A pop-up message should tell you why this option is not available and what to do to make it available again if this is possible.

Best Regards.

II

erik71Author
Associate
October 26, 2025

Hello @Issamos 

In the pop-up message "Ethernet Interface Disabled: Active only if ETH IP is enabled." is written. What does ETH IP mean? I am configuring ETH1 as RGMII mode.

Thank you for your answer.

Ghofrane GSOURI
ST Technical Moderator
October 27, 2025

Hello @erik71 

First let me thank you for posting .

Instead of choosing ETH:RGMII , try to set it as RMII

GhofraneGSOURI_2-1761550911978.png

Then you will become capable to use the ethernet interface option within the NETXDUO

GhofraneGSOURI_3-1761551018541.png

 

In the meantime, I am looking into the reason why the Ethernet interface option in NetX Duo remains grayed out when the ETH interface is configured to use RGMII. I will get back to you asap.

THX

Ghofrane

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
erik71Author
Associate
October 27, 2025

Hello @Ghofrane GSOURI 

 

I'm using the STM32N6570-DK board. This board supports 1GB Ethernet, so I need to configure RGMII.

I need help this.

Thank you for your reply

Ghofrane GSOURI
ST Technical Moderator
October 27, 2025

Hello @erik71 

I confirm that this is a current limitation. An internal ticket (ID: 217238) has been raised and escalated to the development team for further investigation and resolution.

I will keep you posted with updates.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Visitor II
November 4, 2025

Our team is also seeing this issue with Ethernet, joining thread to watch for any updates on this topic