Skip to main content
RCM
Visitor II
November 19, 2018
Question

power consumption of STM32F469NIH? CubeMX or the Data sheet?

Hi, I am looking to calculate the power consumed by the MCU STM32F469NIH. The CubeMX tool has a power consumption calculator with the flexibility to select the peripherals used. Apparently when I calculate using CubeMX with all the peripherals selected, the tool says that MCU consumes 120mA of current. When I check the data sheet the VDD and IDD power lines together consume 390mA of current which is far more than the CubeMX value of 120 mA. I am in a dilemma as to which one of these two sources is close to the real values.

Please help, Your input is much appreciated. Thank you.0690X000006CP3cQAG.jpg0690X000006CP3XQAW.jpg

This topic has been closed for replies.