Associate II
Sep 30, 2021 8:17 AM UTC
Solved
Potential bug for STM32F303 for LL USART and DMA operation
- 1 reply
- 1199 views
Hello,
I created a simple project for a board NUCLEO-F303RE enabling USART2 and DMA for transmit and I believe there is a bug in the code generation that doesn't configure properly the peripherals.
The generated code has:
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_USART2_UART_Init();
MX_TIM2_Init();
MX_DMA_Init();
MX_USART3_UART_Init();
/* USER CODE BEGIN 2 */Then the MX_USART2_UART_Init has:
/* USART2_TX Init */
LL_DMA_SetDataTransferDirection(DMA1, LL_DMA_CHANNEL_7, LL_DMA_DIRECTION_MEMORY_TO_PERIPH);
LL_DMA_SetChannelPriorityLevel(DMA1, LL_DMA_CHANNEL_7, LL_DMA_PRIORITY_LOW);
LL_DMA_SetMode(DMA1, LL_DMA_CHANNEL_7, LL_DMA_MODE_NORMAL);
LL_DMA_SetPeriphIncMode(DMA1, LL_DMA_CHANNEL_7, LL_DMA_PERIPH_NOINCREMENT);
LL_DMA_SetMemoryIncMode(DMA1, LL_DMA_CHANNEL_7, LL_DMA_MEMORY_INCREMENT);
LL_DMA_SetPeriphSize(DMA1, LL_DMA_CHANNEL_7, LL_DMA_PDATAALIGN_BYTE);
LL_DMA_SetMemorySize(DMA1, LL_DMA_CHANNEL_7, LL_DMA_MDATAALIGN_BYTE);
/* USART2 interrupt Init */But it is run BEFORE the MX_DMA_Init, which enables the clock for the DMA:
/* DMA controller clock enable */
LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_DMA1);So I believe this causes the DMA not to get configured properly: I stepped the program during the USART init and the DMA regs are not changing when setting the increment for the memory (Line 10 above).
A quick fix I could do is to copy the DMA Init also before the auto generate inits as in:
/* USER CODE BEGIN SysInit */
MX_DMA_Init(); //Manually copied here too because the clock is not enabled for DMA config done during UART setup
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_USART2_UART_Init();
MX_TIM2_Init();
MX_DMA_Init();
MX_USART3_UART_Init();
/* USER CODE BEGIN 2 */This seems to fix the problem and everything behaves as expected