Skip to main content
Associate
July 31, 2023
Solved

Possible Configuration Issue

Hello,

I am using STM32CubeIDE version 1.13.0 together with STM32CubeMX version 6.9.0-RC9 and the STM32F746IGT6 microcontroller.

I am trying to use TIM2 as a 4 channel Input capture unit, each channel with it's own independent DMA . For this i have the following DMA Streams available:

- DMA1 stream 5 - for TIM2_CH1

- DMA1 stream 6 - for TIM2_CH2/CH4

- DMA1 stream 1 - for TIM2_UP/CH3

- DMA1 stream 7 - for TIM2_UP/CH4

 

The problem i am having is that if I add the DMA1 stream 7 .... stream 6 & stream 1 can no longer be added due to conflicts. In the generated code i see that both events UP & CH4 get linked to this DMA stream so i am guessing that this is why the MX won't let me add the other 2. 

 

Now my question: 

- Even though the tool does not allow it since one trigger can be selected for one DMA tream (Channel selection) i think it should be possible to have the following configuration:

- DMA1 stream 5 - for TIM2 CC1 

- DMA1 stream 6 - for TIM2 CC2

- DMA1 stream 1 - for TIM2 CC3

- DMA1 stream 7 - for TIM2 CC4

Am i correct ?

    This topic has been closed for replies.
    TDK
    TDKBest answer
    July 31, 2023

    Yes, you should be able to get the configuration you want, at least in hardware. It's unclear why CubeMX thinks there is a conflict here, probably a bug.

    "If you feel a post has answered your question, please click ""Accept as Solution""."

    2 replies

    TDK
    TDKBest answer
    July 31, 2023

    Yes, you should be able to get the configuration you want, at least in hardware. It's unclear why CubeMX thinks there is a conflict here, probably a bug.

    "If you feel a post has answered your question, please click ""Accept as Solution""."
    dte1Author
    Associate
    July 31, 2023

    Thank you, figured as much just wanted to be on the safe side and double check.