Skip to main content
chaaalyy
Senior II
Apr 17, 2020 9:15 AM UTC
Question

Possible Bug in cubeMX 5.6.1

Not really an issue, but it is worth mentioning...

inside cubeIDE, i generate a new stm32 project, in target selector i select the nucleo f446re board and initialize it with the standard peripheral settings. When checking the clock configuration, i would expect the HCLK at 180MHz (which is max for that mcu). Unfortunately it´s set to 84MHz, like a f401. It´s no problem to enter just 180 there and let the "Resolve Clock Issues"-Button do the job here, but anyway: it´s a little bit strange ...

Edit: This applies to both versions. cubeMX stand alone and the integrated one in cubeIDE

This topic has been closed for replies.

1 reply

Nesrine.JLASSI
Visitor II
Apr 30, 2020 4:48 AM UTC

Hello @Karl Hönemann​ 

Thanks for the feedback,

Temporarily you have to configure the board manually.

Best regards,

Nesrine