Skip to main content
YiKai
Associate II
Mar 30, 2020 6:41 AM UTC
Question

osKernelStart on STM32 break loop

Hi, I'm use the STM32F429

This is my FREERTOSConfig.h

#define configUSE_PREEMPTION 1
#define configSUPPORT_STATIC_ALLOCATION 0
#define configSUPPORT_DYNAMIC_ALLOCATION 1
#define configUSE_IDLE_HOOK 0
#define configUSE_TICK_HOOK 0
#define configCPU_CLOCK_HZ ( SystemCoreClock )
#define configTICK_RATE_HZ ((TickType_t)1000)
#define configMAX_PRIORITIES ( 7 )
#define configMINIMAL_STACK_SIZE ((uint16_t)128)
#define configTOTAL_HEAP_SIZE ((size_t)15360)
//#define configTOTAL_HEAP_SIZE ((size_t)17*1024)
#define configMAX_TASK_NAME_LEN ( 16 )
#define configUSE_16_BIT_TICKS 0
#define configUSE_MUTEXES 1
#define configQUEUE_REGISTRY_SIZE 8
#define configUSE_PORT_OPTIMISED_TASK_SELECTION 1
 
/* Co-routine definitions. */
#define configUSE_CO_ROUTINES 0
#define configMAX_CO_ROUTINE_PRIORITIES ( 2 )
 
/* Set the following definitions to 1 to include the API function, or zero
to exclude the API function. */
#define INCLUDE_vTaskPrioritySet 1
#define INCLUDE_uxTaskPriorityGet 1
#define INCLUDE_vTaskDelete 1
#define INCLUDE_vTaskCleanUpResources 0
#define INCLUDE_vTaskSuspend 1
#define INCLUDE_vTaskDelayUntil 0
#define INCLUDE_vTaskDelay 1
#define INCLUDE_xTaskGetSchedulerState 1
 
/* Cortex-M specific definitions. */
#ifdef __NVIC_PRIO_BITS
 /* __BVIC_PRIO_BITS will be specified when CMSIS is being used. */
 #define configPRIO_BITS __NVIC_PRIO_BITS
#else
 #define configPRIO_BITS 4
#endif
 
/* The lowest interrupt priority that can be used in a call to a "set priority"
function. */
#define configLIBRARY_LOWEST_INTERRUPT_PRIORITY 15
 
/* The highest interrupt priority that can be used by any interrupt service
routine that makes calls to interrupt safe FreeRTOS API functions. DO NOT CALL
INTERRUPT SAFE FREERTOS API FUNCTIONS FROM ANY INTERRUPT THAT HAS A HIGHER
PRIORITY THAN THIS! (higher priorities are lower numeric values. */
#define configLIBRARY_MAX_SYSCALL_INTERRUPT_PRIORITY 5
 
/* Interrupt priorities used by the kernel port layer itself. These are generic
to all Cortex-M ports, and do not rely on any particular library functions. */
#define configKERNEL_INTERRUPT_PRIORITY 		( configLIBRARY_LOWEST_INTERRUPT_PRIORITY << (8 - configPRIO_BITS) )
/* !!!! configMAX_SYSCALL_INTERRUPT_PRIORITY must not be set to zero !!!!
See http://www.FreeRTOS.org/RTOS-Cortex-M3-M4.html. */
#define configMAX_SYSCALL_INTERRUPT_PRIORITY 	( configLIBRARY_MAX_SYSCALL_INTERRUPT_PRIORITY << (8 - configPRIO_BITS) )

I used the FREERTOS oskerosKernelStart, but it work to some places will be break

osThreadDef(defaultTask, StartDefaultTask, osPriorityNormal, 0, 1024);
defaultTaskHandle = osThreadCreate(osThread(defaultTask), NULL);
/* Start scheduler */
osKernelStart();
while (1)
{
}

void StartDefaultTask(void const * argument)
{  
/* init code for LWIP */
 MX_LWIP_Init();
 tcp_server_init();
 Tcp_Client_Init();
 /* init code for USB_DEVICE */
 MX_USB_DEVICE_Init();
 /* USER CODE BEGIN 5 */
 /* Infinite loop */
 while (1)
 
{	 
osDelay(100);
	 /* USER CODE BEGIN 3 */
	 main_GW();
 }
 

Main_GW is many things to do , I work in StartDefaultTask successfully, but in main_GW it will be break in some place,did have any advise to solve ?

​

​

This topic has been closed for replies.

1 reply

YiKai
YiKaiAuthor
Associate II
Apr 6, 2020 1:26 AM UTC

Thanks all, I change my memory for thread. it is

success to use