Skip to main content
alister
Senior III
Feb 14, 2019 12:57 AM UTC
Question

Organising single software tree for many projects WITHOUT duplicating Drivers/Middlewares

I'd like to organise a software tree that'll accommodate

  • bootloader for a custom board,
  • application for the board,
  • multiple ways of building the application,
  • bootloaders and applications of future "next gen" boards, and
  • a moderate body of application software I'd want to re-use in all the app projects.

I'd like this in a single repository, without duplicating any source files.

I'm using IAR Workbench and/or TrueSTUDIO for STM32.

Both IDEs support

  • multiple projects, i.e. one for each of bootloader for board X, app for board X,
  • multiple build ways, e.g. IAR uses "Configurations" and TrueSTUDIO (Eclipse) uses "Build Configurations", and
  • linking other directories of source files.

The only part I haven't completely solved yet is STM32CubeMX. UM2285 Rev 1 figure 3 shows an .ioc file in a project directory and the Drivers and Middlewares directories it generates located several directories higher at the root of the software tree. Can anyone share how to get STM32CubeMX to generate like this please?

Having Drivers/Middlewares directories duplicated in every project isn't a show-stopper. Just untidy and so I'm wanting to know.

Thanks

Alister

This topic has been closed for replies.

4 replies

Vangelis Fortounas
Associate II
Feb 14, 2019 11:47 PM UTC

hi

In CubeMX, Project manager, Code generator tab check the third option, to add all theese libraries as reference and not copy them.

0690X000006DcH0QAK.jpg

alister
alisterAuthor
Senior III
Feb 15, 2019 12:21 AM UTC

I'd experimented with that and STM32CubeMX generated paths like these in the (IAR) project file:

<state>C:/Users/alister/STM32Cube/Repository/STM32Cube_FW_F7_V1.14.0/Drivers/STM32F7xx_HAL_Driver/Inc</state>
...

The problem here is that other developers cloning or pulling the repository would have different user names.

If you've been here, what was your fix to this?

Thanks

Alister

alister
alisterAuthor
Senior III
Feb 26, 2019 3:51 AM UTC

I've not experimented further with the idea (11 days ago) of changing STM32CubeMX's Firmware Location to point to the root of my software tree.

I'm concerned this may have impacts I'm unaware.

Does anyone have other experience or ideas to share please?

Thanks

Alister