Skip to main content
Ronny Landsverk
Associate III
Aug 27, 2017 8:21 AM UTC
Question

Open/build examples from the CubeMX repository using System Workbench

Posted on August 27, 2017 at 10:21

I use a discovery board, STM32F303VCT6 and the CubeMX / System Workbench for the coding (in C).

If I generate a project via CubeMX, I can open this project and build it in System Workbench - no problems.

In CubeMX I have installed library: Firmware Package for Family STM32F3 - version 1.9.0 which downloads a zipped folder in the CubeMX repository path.

This zipped folder contains examples and demonstrations which I wish to test. Following the Getting started with STMCubeF3, I try to open the GPIO_EXTI example project.

I set the workspace using the Switch Workspace >> Other command in System Workbench.

From the Getting started - guide, you should browse to the SW4STM32 directory and open the project using Import >> Existing Project into Workspace. Whatever project I try to open and build, I get Fatal Error: stm32f3xx_hal.h: No such file or directory. I follow the instructions from the Getting started - guide (point by point, exactly),...  I try to copy the stm32f3xx_hal.h file to the workspace, but still I get this problem.

Please guide me as I am in the early stages of understanding the STM32 toolchain and I am not a CS expert. In particular I am not so familiar with CS jargon.

#cubemx-repository-example-projects
This topic has been closed for replies.

1 reply

Ronny Landsverk
Associate III
Aug 27, 2017 10:16 AM UTC
Posted on August 27, 2017 at 12:16

The problem was that I copied the STM32F3-Discovery - folder to a different location, to avoid messing up the original files. In doing this, I missed the drivers located two levels above... If you have similar problem, be sure to copy the folder-structure from the STM32Cube_FW_F3_V1.9.0 - folder and not as shown in the Getting started with STMCube F3, figure 4 - where the figure shows the folder-structure two levels to deep...