Skip to main content
Associate III
Jul 6, 2026 6:21 PM UTC
Solved

NX_SECURE_TLS_TLS_1_2_ENABLED and NX_SECURE_TLS_TLS_1_3_ENABLED should not be available as check boxes in STM32CubeMX

STM32CubeMX 6.18.0

MCU: STM32H563RIT6

To my understanding, this uses STM32CubeH5 1.7.0

 

Start a new project and enable ThreadX and NetX Duo.

In “NETXDUO Mode and Configuration”, enable “NX Core”, “Crypto” and “TLS”

In configuration, parameter column “NetXDuo” there are check-boxes for:

TLS CORE

NX_SECURE_TLS_ENABLE_TLS_1_1

NX_SECURE_TLS_ENABLE_TLS_1_3

NX_SECURE_TLS_TLS_1_2_ENABLED

NX_SECURE_TLS_TLS_1_3_ENABLED

 

This is a bug.

According to https://github.com/eclipse-threadx/rtos-docs/blob/1e36a62618de3771c973196e7648cba50d19cf1f/rtos-docs/netx-duo/netx-duo-secure-tls/chapter2.md#configuration-options the proper configuration options are

NX_SECURE_TLS_ENABLE_TLS_1_3 Defined, this option enables TLSv1.3 mode. TLS 1.3 is the newest version of TLS and is disabled by default.
NX_SECURE_TLS_ENABLE_TLS_1_0 Defined, this option enables the legacy TLSv1.0 mode. TLSv1.0 is considered obsolete so it should only be enabled for backward-compatibility with older applications.
NX_SECURE_TLS_ENABLE_TLS_1_1 Defined, this option enables the legacy TLSv1.1 mode. TLSv1.1 is considered obsolete so it should only be enabled for backward-compatibility with older applications.

 

NX_SECURE_TLS_TLS_1_2_ENABLED and NX_SECURE_TLS_TLS_1_3_ENABLED (and other preprocessor identifiers named *_TLS_TLS_*) are internal to NetXDuo and should not be touched from outside or provided as compiler arguments. They are set in Middlewares/ST/netxduo/nx_secure/inc/nx_secure_tls.h from the NX_SECURE_TLS_ENABLE_TLS_1_1 and NX_SECURE_TLS_ENABLE_TLS_1_3.

Note that checking NX_SECURE_TLS_TLS_1_2_ENABLED and NX_SECURE_TLS_TLS_1_3_ENABLED doesn’t actually affect the generated code (at least for STM32CubeIDE). Only .mxproject and the .ioc-file are changed.

But it is confusing for the developers. Especially since the latter options do not actually do anything. So they should be removed from the UI.

   Best regards, Jesper

 

Ghofrane GSOURI
Ghofrane GSOURIBest answer
ST Technical Moderator
Jul 7, 2026 7:32 AM UTC

Hello ​@JesperEC 

Your detailed explanation is much appreciated.

Issue has been escalated to dev team under internal ticket ID #0064181  for further investigation.

I will keep you posted with updates.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

1 reply

Ghofrane GSOURI
Ghofrane GSOURIBest answer
ST Technical Moderator
Jul 7, 2026 7:32 AM UTC

Hello ​@JesperEC 

Your detailed explanation is much appreciated.

Issue has been escalated to dev team under internal ticket ID #0064181  for further investigation.

I will keep you posted with updates.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.