Skip to main content
Associate
July 7, 2025
Question

[Nucleo-n6570-q] About XSPI LR can't run in SYSB at 400MHZ when number of memory data lines set 8line

Hello, 

I'm learning about the STM32N6 LR and XIP examples and want to get hands-on with them. I've already set OTP124 to 0x8000.

bioak_0-1751875928615.png

 

If SYSB is configured to 400MHz, the number of memory data lines must be set to 1 line and disable "X_ICACHE_Init()" for the app to function.

bioak_1-1751877350600.png

 

However, if SYSB is set to 80MHz, the number of memory data lines can be configured to 8 lines  and disable "X_ICACHE_Init()", and the app still works.

bioak_2-1751877530482.png

 

I'm very confused by this result and wonder if anyone has encountered the same problem or knows what I should modify?

Thank you.

This topic has been closed for replies.