Skip to main content
KevinA
Senior
Jun 6, 2018 1:32 AM UTC
Question

NUCLEO-L476RG and X-NUCLEO-53L1A1 Working together

Posted on June 06, 2018 at 03:32

I ordered and received NUCLEO-L476RG and X-NUCLEO-53L1A1, in the X-NUCLEO-53L1A1 they had and 'expandsion pack' for STM32Cube but when I click on the Additional Software Components selection there is no means to add the code for the 53L1A1.

How does this all work?

#stm32cubemx
This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
Jun 6, 2018 1:45 AM UTC
Posted on June 06, 2018 at 03:45

Despite the name they are not extensions to CubeMX

They are basically standalone HAL example projects that will build on a number of tool chains.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Bogdan Golab
Lead
Jun 6, 2018 4:57 AM UTC
Posted on June 06, 2018 at 06:57

I have an older version X-NUCLEO-53L0A1. As far as I remember there were examples for the nucleo board you have in the software pack.

And also for nucleo-F401.

So manual integration is required if you want to add the module to other nucleo  board or enable other MCU resources using CubeMX.