Skip to main content
mbarg.1
Senior III
Apr 29, 2021 7:12 AM UTC
Question

Nucleo-H753ZI BUG in default configuration

TM32Cube ver 1.6.1 MX ver 6.2.1 with STM32Cube_FW_H7_V1.9.0 - select Nucleo-H753ZI with default configuration and generate new project - add some activity like

HAL_GPIO_WritePin(GPIOB, LD3_Pin, GPIO_PIN_SET);

HAL_Delay(1000);

HAL_GPIO_WritePin(GPIOB, LD3_Pin, GPIO_PIN_RESET);

HAL_Delay(1000);

in while loop ( after USER CODE BEGIN 3).

NOT WORKING

From debug, system hangs up in MX_USART3_UART_Init() ==> HAL_UART_Init() ==> UART_CheckIdleState() ==> UART_WaitOnFlagUntilTimeout() ...

Disable USART3 and it works.

Or change UART clock to 8M (automatic clock fixing gives 32M) and it works.

Please fix it.

Mike Bargauan

This topic has been closed for replies.

6 replies

Khouloud OTHMAN
Associate
May 21, 2021 6:20 PM UTC

Hello @mbarg.1​,

First let le welcome you to our STM32 community :smiling_face_with_smiling_eyes:

Please excuse the somewhat late reply and thank you for having reported.

Actually I can't reproduce the issue from my side. Could you please share your .ioc file for further check?

Thanks in advance.

Khouloud.

mbarg.1
mbarg.1Author
Senior III
May 22, 2021 1:23 PM UTC
Khouloud: due to size limitation in my system, I will send you several mail, each with a different file. First is the project as it get out of my system when I do select nucleo-H573ZI board. Mike ---------------------------- Original Message ---------------------------- Subject: Khouloud OTHMAN mentioned you in an answer to: Nucleo-H753ZI BUG in default configuration From: "ST Community" Date: Fri, May 21, 2021 6:20 pm To: "mikebargauan@mb-international.com"