Skip to main content
Asantos
Associate III
Jan 9, 2019 11:56 PM UTC
Question

NUCLEO-H743ZI USB Host HID. Has anyone ever made it work?

Hi,

I'm trying to create a project to test the USB Host in HID keybord mode using the NUCLEO-H743ZI board. My keybord worked in the STM32H743-EVAL board and the STM32Cube_FW_H7_V1.3.0 USB Host HID example.

 I noted that the Eval board example code generate an OTG_FS_IRQ just after the "USBH_Start(&hUSBHost)" function call. Only if the Keyboard is attached. My project runing in the NUCLEO-H743ZI don't trigger the ISR. 

What could be wrong with my CubeMx V4.27 configuration?

This topic has been closed for replies.

5 replies

Mon2
Senior III
Jan 10, 2019 4:04 AM UTC

CubeMX is currently @ 5.0.1 release. Consider to upgrade your toolchain and test again.

Asantos
AsantosAuthor
Associate III
Jan 10, 2019 2:58 PM UTC

 I made it work using the STM32H743I-EVAL and CubeMX V4.27. Anyway I did the upgrade for the V5.01 and still not working for the NUCLEO-H743ZI, I tested in two different boards. So I think that it is a specific board configuration issue.

 LED 8 is lighting, so there is power in Vbus.

Has someone already made USB Host HID work for NUCLEO-H743ZI?

Mon2
Senior III
Jan 10, 2019 4:22 PM UTC

Have you seen this?

https://community.st.com/s/question/0D50X00009cd6whSAA/usb-hid-host-connect?

From the following document:

STM32CubeH7 Firmware Examples for STM32H7xx Series

The USB HOST HID IP is supported on the STM32H743I-EVAL but not on the NUCLEO-H743ZI so there is some minor difference to prevent the use of the same code run on the NUCLEO target.

0690X000006D2IdQAK.png

Asantos
AsantosAuthor
Associate III
Jan 11, 2019 12:20 AM UTC

Thanks for the hint Mon2.

I think that the NUCLEO-H743ZI board is capable to run an USB Host HID application. The problem is that ST examples use the LCD to show devices inputs and status. They should have done examples for the NUCLEO boards, where the device inputs (Keyboard or Mouse) is stored in a buffer.

flyer31
Senior
Jan 12, 2019 10:13 PM UTC

I got the Nucleo H734 run nicely in USB Device mode based on the CDC_Standalone, even now my own application in HS Mode with ULPI and USB3300 USB chip ... but I needed some days to strip it away of the HAL stuff, this HAL stuff in my eyes is really terrible - it somehow tries to hide all details of the processor, but in fact it makes all much more complicated ... it is all inter-connected in some terribly undocumented way in the lower levels, even using very crazy macro programming... . Somehow some people seemed to think that they make it all easy, if they hide the processor, but they forget that the reference manual is > 1000 pages strong, and if they wan to hide this, they would at least need > 1000 pages of detail description of their "nice new world" HAL invention ... I think nobody really wants this ... .

But the programming of the USB itself seems to be nice, much nicer and clearer than the USB for STM32F4 ... somehow similar basic functions but much clearer strcutured... but you need some time for all this ... maybe you can help to convice STM to present some "non-HAL" simple demo programs (which first requires a simple and slim STM32H743xx.h...).