Skip to main content
October 28, 2019
Question

Not running NAND FLASH with STM32H70VB

  • October 28, 2019
  • 1 reply
  • 597 views

Hi,

I have a Project which is about data transfering and storaging.

I use STM32H750VB micro processor, MT29F32G08CBADBWP-12IT:D Nand Flash and LAN8742A Ethernet Chip for my application.

I configure and run Ethernet, ADC, I/O, UART etc. functions with using CubeMX. However I had some problems on Nand Flash application while was trying tu run it.

I did run the Nand Flash application correct when I used STM32F407 Discovery MB997B development kit.

I couldn’t find yet any example about H743ZI development kit.

1-     Do you have any experience about programming Nand Flash application with using H743ZI development kit.

2-     Do you have any idea "MPU - Memory Protection Unit" inside micro processor.

This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
November 11, 2019

Think you're going to need to own the coding/porting of drivers for this. People generally have migrated to eMMC to solve a host of issues from EOL form factors, architecture/geometry issues, and wear levelling.

​

Yes, you probably want to use the MPU, don't want buffering or caching on NAND space. Review books or manuals on CM7 core, or CPU architecture/design, if unfamiliar with the topic area.​

​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..