Not getting all ADC end of conversion interrupts
- 2 replies
- 2071 views
I'm using the STM32L475 processor with STM32CubeMX 6.11.1.
I have configured ADC1 to read two channels, an external input and the internal temperature - see configuration image in CubeMX. The code to drive the adc reading is simple:
int16_t Channel;
void Adc_Convert(void)
{
Channel = 0;
if (HAL_ADC_Start_IT(&hadc1) != HAL_OK)
{
for(;;) ;
}
}
void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef * hadc)
{
Adc.Result[Channel] = HAL_ADC_GetValue(hadc);
Channel++;
}
void HAL_ADC_ErrorCallback(ADC_HandleTypeDef * hadc)
{
uint32_t err = HAL_ADC_GetError(hadc);
}
Adc_Convert() is called once every 2 seconds. I only ever get 1 end-of-conversion interrupt, so the temeprature input is never being read - I can see this both by looking at the Adc.Result array and by using breakpoints to confirm. HAL_ADC_ErrorCallbackI() is never called.
This seems quite a minimal example of trying to use the ADC with interrupts, so what is going on?
All suggestions or help appreciated.