Skip to main content
SS.Sagar
Associate III
May 7, 2019 1:09 PM UTC
Question

Not able to get the truestudio working with cubemx

Hi,

I am using cubemx for code generation and i have atollic compiler.

This is first time i am using atollic, previous to that i was using keil and now i have started to use ubuntu. so no keil for ubuntu.

when i generate the code with cubemx, i don't see any makefile there and not project files.

do i need to write makefiles manually?

i googled for the same but didn't get much help.

This topic has been closed for replies.

1 reply

Markus GIRDLAND
ST Employee
May 9, 2019 1:42 PM UTC

You can generate a project for TrueSTUDIO and then import it and then you're pretty much done and ready to go.

My colleague Mattias did a video that's slightly outdated (new MX design) but it should give you a good idea of how to do it.

You can find it here.