Skip to main content
polgu.1
Associate II
Jun 16, 2022 4:58 PM UTC
Question

Need help to read Accelerometer with I2C DMA

I'm try to read acceleration from KX132 accelerometer with a STM32F446ZE through I2C with DMA. I create a project with STMCubeMX and enable DMA and interruptions.

The accelerometer has six register each one of 1 byte where save acceleration in this format: XOUT_L,XOUT_H, YOUT_L, YOUT_H, ZOUT_L, ZOUT_H.

​

I want to read this registers continously with I2C DMA but I have a problem, only can read once time and never jump the complete transfer interruption again. I'll leave parts of my code so you can understand what i'm doing.

​

This configuration it was create by STMCubeMX. I choose DMA_CIRCULAR mode to repeat reading by DMA but doesn't work.

​

i2c.c

/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "i2c.h"
 
/* USER CODE BEGIN 0 */
 
/* USER CODE END 0 */
 
I2C_HandleTypeDef hi2c2;
DMA_HandleTypeDef hdma_i2c2_rx;
DMA_HandleTypeDef hdma_i2c2_tx;
 
/* I2C2 init function */
void MX_I2C2_Init(void)
{
 
 /* USER CODE BEGIN I2C2_Init 0 */
 
 /* USER CODE END I2C2_Init 0 */
 
 /* USER CODE BEGIN I2C2_Init 1 */
 
 /* USER CODE END I2C2_Init 1 */
 hi2c2.Instance = I2C2;
 hi2c2.Init.ClockSpeed = 100000;
 hi2c2.Init.DutyCycle = I2C_DUTYCYCLE_2;
 hi2c2.Init.OwnAddress1 = 0;
 hi2c2.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
 hi2c2.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
 hi2c2.Init.OwnAddress2 = 0;
 hi2c2.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
 hi2c2.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
 if (HAL_I2C_Init(&hi2c2) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN I2C2_Init 2 */
 
 /* USER CODE END I2C2_Init 2 */
 
}
 
void HAL_I2C_MspInit(I2C_HandleTypeDef* i2cHandle)
{
 
 GPIO_InitTypeDef GPIO_InitStruct = {0};
 if(i2cHandle->Instance==I2C2)
 {
 /* USER CODE BEGIN I2C2_MspInit 0 */
 
 /* USER CODE END I2C2_MspInit 0 */
 
 __HAL_RCC_GPIOF_CLK_ENABLE();
 /**I2C2 GPIO Configuration
 PF0 ------> I2C2_SDA
 PF1 ------> I2C2_SCL
 */
 GPIO_InitStruct.Pin = GPIO_PIN_0|GPIO_PIN_1;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_OD;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
 GPIO_InitStruct.Alternate = GPIO_AF4_I2C2;
 HAL_GPIO_Init(GPIOF, &GPIO_InitStruct);
 
 /* I2C2 clock enable */
 __HAL_RCC_I2C2_CLK_ENABLE();
 
 /* I2C2 DMA Init */
 /* I2C2_RX Init */
 hdma_i2c2_rx.Instance = DMA1_Stream2;
 hdma_i2c2_rx.Init.Channel = DMA_CHANNEL_7;
 hdma_i2c2_rx.Init.Direction = DMA_PERIPH_TO_MEMORY;
 hdma_i2c2_rx.Init.MemBurst = DMA_MBURST_SINGLE;
 hdma_i2c2_rx.Init.PeriphInc = DMA_PINC_ENABLE;
 hdma_i2c2_rx.Init.MemInc = DMA_MINC_ENABLE;
 hdma_i2c2_rx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
 hdma_i2c2_rx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
 hdma_i2c2_rx.Init.Mode = DMA_CIRCULAR;
 hdma_i2c2_rx.Init.PeriphBurst = DMA_PBURST_SINGLE;
 hdma_i2c2_rx.Init.PeriphInc = DMA_PINC_DISABLE;
 hdma_i2c2_rx.Init.Priority = DMA_PRIORITY_HIGH;
 hdma_i2c2_rx.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
 if (HAL_DMA_Init(&hdma_i2c2_rx) != HAL_OK)
 {
 Error_Handler();
 }
 
 __HAL_LINKDMA(i2cHandle,hdmarx,hdma_i2c2_rx);
 
 /* I2C2_TX Init */
 hdma_i2c2_tx.Instance = DMA1_Stream7;
 hdma_i2c2_tx.Init.Channel = DMA_CHANNEL_7;
 hdma_i2c2_tx.Init.Direction = DMA_MEMORY_TO_PERIPH;
 hdma_i2c2_tx.Init.PeriphInc = DMA_PINC_DISABLE;
 hdma_i2c2_tx.Init.MemInc = DMA_MINC_ENABLE;
 hdma_i2c2_tx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
 hdma_i2c2_tx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
 hdma_i2c2_tx.Init.Mode = DMA_CIRCULAR;
 hdma_i2c2_tx.Init.Priority = DMA_PRIORITY_LOW;
 hdma_i2c2_tx.Init.FIFOMode = DMA_FIFOMODE_ENABLE;
 if (HAL_DMA_Init(&hdma_i2c2_tx) != HAL_OK)
 {
 Error_Handler();
 }
 
 __HAL_LINKDMA(i2cHandle,hdmatx,hdma_i2c2_tx);
 
 /* I2C2 interrupt Init */
 HAL_NVIC_SetPriority(I2C2_EV_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(I2C2_EV_IRQn);
 HAL_NVIC_SetPriority(I2C2_ER_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(I2C2_ER_IRQn);
 /* USER CODE BEGIN I2C2_MspInit 1 */
 
 /* USER CODE END I2C2_MspInit 1 */
 }
}
 
void HAL_I2C_MspDeInit(I2C_HandleTypeDef* i2cHandle)
{
 
 if(i2cHandle->Instance==I2C2)
 {
 /* USER CODE BEGIN I2C2_MspDeInit 0 */
 
 /* USER CODE END I2C2_MspDeInit 0 */
 /* Peripheral clock disable */
 __HAL_RCC_I2C2_CLK_DISABLE();
 
 /**I2C2 GPIO Configuration
 PF0 ------> I2C2_SDA
 PF1 ------> I2C2_SCL
 */
 HAL_GPIO_DeInit(GPIOF, GPIO_PIN_0);
 
 HAL_GPIO_DeInit(GPIOF, GPIO_PIN_1);
 
 /* I2C2 DMA DeInit */
 HAL_DMA_DeInit(i2cHandle->hdmarx);
 HAL_DMA_DeInit(i2cHandle->hdmatx);
 
 /* I2C2 interrupt Deinit */
 HAL_NVIC_DisableIRQ(I2C2_EV_IRQn);
 HAL_NVIC_DisableIRQ(I2C2_ER_IRQn);
 /* USER CODE BEGIN I2C2_MspDeInit 1 */
 
 /* USER CODE END I2C2_MspDeInit 1 */
 }
}
 
/* USER CODE BEGIN 1 */
 
/* USER CODE END 1 */

Set DMA interruptions.

​

dma.c

/* USER CODE BEGIN 0 */
 
/* USER CODE END 0 */
 
/*----------------------------------------------------------------------------*/
/* Configure DMA */
/*----------------------------------------------------------------------------*/
 
/* USER CODE BEGIN 1 */
 
/* USER CODE END 1 */
 
/**
 * Enable DMA controller clock
 */
void MX_DMA_Init(void)
{
 
 /* DMA controller clock enable */
 __HAL_RCC_DMA1_CLK_ENABLE();
 
 /* DMA interrupt init */
 /* DMA1_Stream2_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(DMA1_Stream2_IRQn, 6, 0);
 HAL_NVIC_EnableIRQ(DMA1_Stream2_IRQn);
 /* DMA1_Stream7_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(DMA1_Stream7_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(DMA1_Stream7_IRQn);
 
}
 
/* USER CODE BEGIN 2 */
 
/* USER CODE END 2 */

​

I use HAL_I2C_Mem_Read_DMA() because i can select the register from accelerometer it save the accelerations. When I run this code in debug mode, HAL_I2C_Mem_Read_DMA() works fine and I can read 6 bytes of acceleration on rxData1

​enter to while(1) and stop in HAL_Delay(50). After that, jump to DMA Interruption on stm32f4xx_it.c specifically on DMA1_Stream2_IRQHandler() function (describes below). Here excecute HAL_DMA_IRQHandler(&hdma_i2c2_rx) and go to HAL_I2C_MemRxCpltCallback(I2C_HandleTypeDef *hi2c2) describe in main.c. After all that the code come back to HAL_Delay(50) from while(1) and never go jump to interrupt for refresh data from accelerometer.

I hope you can help me. I'm not sure if I'm doing it right, if you have a tips it will be hopeful for me or if you need more information feel free to ask me.

This topic has been closed for replies.

1 reply

polgu.1
polgu.1Author
Associate II
Jun 16, 2022 4:59 PM UTC

More code...

main.c 

#include "stdio.h"
#include "main.h"
#include "dma.h"
#include "i2c.h"
#include "gpio.h"
 
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#define KX132_ADDRESS 0x1E
#define READ 0x01
#define WRITE 0x00
#define RX_BUFF_LEN 12
uint8_t BUFF_ADDRESS = 0x63;
uint8_t XOUT_L = 0x08;
static uint8_t rxData1[RX_BUFF_LEN];
 
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
 
/* USER CODE END PTD */
 
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
 
/* USER CODE END PD */
 
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
 
/* USER CODE END PM */
 
/* Private variables ---------------------------------------------------------*/
 
/* USER CODE BEGIN PV */
 
/* USER CODE END PV */
 
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
 
/* USER CODE BEGIN PFP */
 
/* USER CODE END PFP */
 
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
 
/* USER CODE END 0 */
 
#define RX_BUFF_LEN 12
static uint8_t rxData1[RX_BUFF_LEN];
 
extern DMA_HandleTypeDef hdma_i2c2_rx;
 
int main(void)
{
 /* USER CODE BEGIN 1 */
 
 /* USER CODE END 1 */
 
 /* MCU Configuration--------------------------------------------------------*/
 
 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();
 
 /* USER CODE BEGIN Init */
 
 /* USER CODE END Init */
 
 /* Configure the system clock */
 SystemClock_Config();
 
 /* USER CODE BEGIN SysInit */
 
 /* USER CODE END SysInit */
 
 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_DMA_Init();
 MX_I2C2_Init();
 
 /* USER CODE BEGIN 2 */
 
 /* USER CODE END 2 */
 
 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 
 HAL_I2C_Mem_Read_DMA(&hi2c2, (uint16_t)(KX132_ADDRESS << 1) | READ, XOUT_L, 1, (uint8_t *)rxData1, 6);
 
 while (1)
 {
 
 HAL_Delay(50);
 
 }
 
 /* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
 
void HAL_I2C_MemTxCpltCallback(I2C_HandleTypeDef *hi2c2)
{
 /* Toggle LED: Transfer in transmission process is correct */
 HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_8);
}
 
void HAL_I2C_MemRxCpltCallback(I2C_HandleTypeDef *hi2c2)
{
 /* Toggle LED: Transfer in transmission process is correct */
 HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_8);
}
 
void HAL_I2C_ErrorCallback(I2C_HandleTypeDef *I2cHandle)
{
 /* Turn LED3 on: Transfer error in reception/transmission process */
 HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_8);
}
 
/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
 
 /** Configure the main internal regulator output voltage
 */
 __HAL_RCC_PWR_CLK_ENABLE();
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
 
 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
 RCC_OscInitStruct.HSIState = RCC_HSI_ON;
 RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
 RCC_OscInitStruct.PLL.PLLM = 8;
 RCC_OscInitStruct.PLL.PLLN = 180;
 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
 RCC_OscInitStruct.PLL.PLLQ = 2;
 RCC_OscInitStruct.PLL.PLLR = 2;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }
 
 /** Activate the Over-Drive mode
 */
 if (HAL_PWREx_EnableOverDrive() != HAL_OK)
 {
 Error_Handler();
 }
 
 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_SYSCLK | RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;
 
 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5) != HAL_OK)
 {
 Error_Handler();
 }
}
 
/* USER CODE BEGIN 4 */
 
/* USER CODE END 4 */
 
/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}
 
#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * @param file: pointer to the source file name
 * @param line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
 

DMA Interruption

stm32f4xx_it.c

/* USER CODE END Header */
 
/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "stm32f4xx_it.h"
 
/* External variables --------------------------------------------------------*/
extern DMA_HandleTypeDef hdma_i2c2_rx;
extern DMA_HandleTypeDef hdma_i2c2_tx;
extern I2C_HandleTypeDef hi2c2;
 
/******************************************************************************/
/* Cortex-M4 Processor Interruption and Exception Handlers */
/******************************************************************************/
/**
 
/******************************************************************************/
/* STM32F4xx Peripheral Interrupt Handlers */
/* Add here the Interrupt Handlers for the used peripherals. */
/* For the available peripheral interrupt handler names, */
/* please refer to the startup file (startup_stm32f4xx.s). */
/******************************************************************************/
 
/**
 * @brief This function handles DMA1 stream2 global interrupt.
 */
void DMA1_Stream2_IRQHandler(void)
{
 /* USER CODE BEGIN DMA1_Stream2_IRQn 0 */
 
 /* USER CODE END DMA1_Stream2_IRQn 0 */
 
 HAL_DMA_IRQHandler(&hdma_i2c2_rx);
 
 /* USER CODE BEGIN DMA1_Stream2_IRQn 1 */
 
 /* USER CODE END DMA1_Stream2_IRQn 1 */
}
 
/**
 * @brief This function handles DMA1 stream7 global interrupt.
 */
void DMA1_Stream7_IRQHandler(void)
{
 /* USER CODE BEGIN DMA1_Stream7_IRQn 0 */
 
 /* USER CODE END DMA1_Stream7_IRQn 0 */
 HAL_DMA_IRQHandler(&hdma_i2c2_tx);
 /* USER CODE BEGIN DMA1_Stream7_IRQn 1 */
 
 /* USER CODE END DMA1_Stream7_IRQn 1 */
}
 
/* USER CODE BEGIN 1 */
 
/* USER CODE END 1 */