Question
Multiple ADC Channel Configuration Issue With STM32H723ZG nucleo board
- 2 replies
- 1227 views
Hello STM Team,
I am using the STM32H723ZG board with MATLAB STM embedded coder support packages and I configured the STM32H7 MCU peripherals for ADC1,ADC2 and ADC3,PWM and GPIO, i can see the signals on the GPIO output pins and PWM when I don't use the multiple configuration's in the ADC but When I configure the Multiple channel ADC configuration, I could not see any signal on the GPIO and PWM pins, Can i know is there any issue with DMA configuration with Multiple channel ADC?
Attached the multiple channel configurations for ADC in the picture.
BR
Venkat