Skip to main content
Associate
December 15, 2025
Question

Misleading Warnings

Hi,

Recently, updated to 6.16.1 on Linux.

On a fresh project i get the "misconfiguration warning" when i hit "GENERATE CODE" (I use CMake Toolchain). See Screenshot: There you will see simple config for RCC. Got a "green check" symbol but i always get that Warning.

On the second Screenshot, I have changed OCTOSPI settings, and it will add itself to the Warning list. I can extend the warning list by just changing any settings. Maybe I really misconfigured something, but I don't see it.

I guess it is a bug - I can generate the code, but this Warning might mask real configuration issues in the future.

Thx

2 replies

ST Technical Moderator
December 15, 2025

Hello @b3rtl 

Thank you for posting!

Could you add some details about your issue, The MCU used? version of OS (Fedora, ubuntu, etc)?

I will check this matter with dedicated team and get back to you ASAP.

KR, Souhaib

To give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
b3rtlAuthor
Associate
December 15, 2025

Hi,

I use Debian 12 - You can see the MCU in the Screenshot (H7A3AIIxQ).

New info: After changing some more settings, the issue resolved magically. But I can't say which one did it. I can only confirm it is not any clock configuration - only Pinout&Configuration. What I've changed else afterwards: Enabled FreeRtos, Enabled also OCTOSPI2, I2C1, Enabled one EXTI Pin, USART1, and set TIM7 at "SYS". That's it, it resolved but it might confuse or annoy other users, who start a fresh project.

Thx