Skip to main content
Aasdf.3
Associate
Feb 2, 2021 9:28 AM UTC
Solved

MII on STM32H730VBTx

STM32CubeMX doesn't show MII as an option for Ethernet on the STM32H730VBTx. Is MII not available on this part (RMII only?) or is there a problem with STM32CubeMX? The datasheet suggests it should support MII.

This topic has been closed for replies.
Khouloud ZEMMELI
Khouloud ZEMMELIBest answer
ST Employee
Feb 2, 2021 11:00 AM UTC

Hello @Community member​ 

Thanks for your question,

Yes, the MII is supported on STM32H730xB but not on all Package, in fact, the H740VBTx has the LQFP100 package and the signals needed to reach the MII mode are not all available on it.

Here, I'm talking about the ETH_MII_TX_CLK signal which is not supported on LQFP100 and therfore the MII is not supported.

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Thanks, Khouloud

2 replies

Khouloud ZEMMELI
Khouloud ZEMMELIBest answer
ST Employee
Feb 2, 2021 11:00 AM UTC

Hello @Community member​ 

Thanks for your question,

Yes, the MII is supported on STM32H730xB but not on all Package, in fact, the H740VBTx has the LQFP100 package and the signals needed to reach the MII mode are not all available on it.

Here, I'm talking about the ETH_MII_TX_CLK signal which is not supported on LQFP100 and therfore the MII is not supported.

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Thanks, Khouloud

Aasdf.3
Aasdf.3Author
Associate
Feb 4, 2021 6:33 AM UTC

Thanks for the help.