Skip to main content
NSemrHomeInit
Associate III
Dec 5, 2020 2:52 PM UTC
Question

Message error after generation of default project for STM32F429I for FreeRTOS

Dear ST Hello,

I am using Cubmx to create an RTOS for stm32f429I discovery board.

I generated the default project for this board with FreeRTOS.

I have an error compilation,

Middlewares/Third_Party/FreeRTOS/Source/tasks.o: In function `prvAddNewTaskToReadyList':

C:/Users/STarikUser/STM32CubeIDE/workspace_1.3.0/TS_RtosForTrace/Debug/../Middlewares/Third_Party/FreeRTOS/Source/tasks.c:1127: undefined reference to `prvTraceGetObjectHandle'

C:/Users/STarikUser/STM32CubeIDE/workspace_1.3.0/TS_RtosForTrace/Debug/../Middlewares/Third_Party/FreeRTOS/Source/tasks.c:1127: undefined reference to `prvTraceSetTaskNumberLow16'

C:/Users/STarikUser/STM32CubeIDE/workspace_1.3.0/TS_RtosForTrace/Debug/../Middlewares/Third_Party/FreeRTOS/Source/tasks.c:1127: undefined reference to `prvTraceSetTaskNumberHigh16'

C:/Users/STarikUser/STM32CubeIDE/workspace_1.3.0/TS_RtosForTrace/Debug/../Middlewares/Third_Party/FreeRTOS/Source/tasks.c:1127: undefined reference to `prvTraceGetTaskNumberLow16'

C:/Users/STarikUser/STM32CubeIDE/workspace_1.3.0/TS_RtosForTrace/Debug/../Middlewares/Third_Party/FreeRTOS/Source/tasks.c:1127: undefined reference to `prvTraceSetObjectName'

C:/Users/STarikUser/STM32CubeIDE/workspace_1.3.0/TS_RtosForTrace/Debug/../Middlewares/Third_Party/FreeRTOS/Source/tasks.c:1127: undefined reference to `prvTraceGetTaskNumberLow16'

C:/Users/STarikUser/STM32CubeIDE/workspace_1.3.0/TS_RtosForTrace/Debug/../Middlewares/Third_Party/FreeRTOS/Source/tasks.c:1127: undefined reference to `prvTraceSetPriorityProperty'

C:/Users/STarikUser/STM32CubeIDE/workspace_1.3.0/TS_RtosForTrace/Debug/../Middlewares/Third_Party/FreeRTOS/Source/tasks.c:1127: undefined reference to `prvTraceGetCurrentTaskHandle'

C:/Users/STarikUser/STM32CubeIDE/workspace_1.3.0/TS_RtosForTrace/Debug/../Middlewares/Third_Party/FreeRTOS/Source/tasks.c:1127: undefined reference to `prvTraceGetTaskNumberHigh16'

C:/Users/STarikUser/STM32CubeIDE/workspace_1.3.0/TS_RtosForTrace/Debug/../Middlewares/Third_Party/FreeRTOS/Source/tasks.c:1127: undefined reference to `prvTraceGetTaskNumberHigh16'

C:/Users/STarikUser/STM32CubeIDE/workspace_1.3.0/TS_RtosForTrace/Debug/../Middlewares/Third_Party/FreeRTOS/Source/tasks.c:1127: undefined reference to `prvTraceGetTaskNumberLow16'

C:/Users/STarikUser/STM32CubeIDE/workspace_1.3.0/TS_RtosForTrace/Debug/../Middlewares/Third_Party/FreeRTOS/Source/tasks.c:1127: undefined reference to `prvTraceStoreKernelCall'

C:/Users/STarikUser/STM32CubeIDE/workspace_1.3.0/TS_RtosForTrace/Debug/../Middlewares/Third_Party/FreeRTOS/Source/tasks.c:1127: undefined reference to `prvAddTaskToStackMonitor'

C:/Users/STarikUser/STM32CubeIDE/workspace_1.3.0/TS_RtosForTrace/Debug/../Middlewares/Third_Party/FreeRTOS/Source/tasks.c:1129: undefined reference to `prvTraceGetTaskNumberHigh16'

C:/Users/STarikUser/STM32CubeIDE/workspace_1.3.0/TS_RtosForTrace/Debug/../Middlewares/Third_Party/FreeRTOS/Source/tasks.c:1129: undefined reference to `prvTraceGetTaskNumberLow16'

C:/Users/STarikUser/STM32CubeIDE/workspace_1.3.0/TS_RtosForTrace/Debug/../Middlewares/Third_Party/FreeRTOS/Source/tasks.c:1129: undefined reference to `prvTraceStoreTaskReady'

C:/Users/STarikUser/STM32CubeIDE/workspace_1.3.0/TS_RtosForTrace/Debug/../Middlewares/Third_Party/FreeRTOS/Source/tasks.c:1152: undefined reference to `CurrentFilterGroup'

C:/Users/STarikUser/STM32CubeIDE/workspace_1.3.0/TS_RtosForTrace/Debug/../Middlewares/Third_Party/FreeRTOS/Source/tasks.c:1152: undefined reference to `CurrentFilterMask'

Thank you in advance,

S.Tarik,

This topic has been closed for replies.

5 replies

Khouloud ZEMMELI
ST Employee
Dec 7, 2020 7:20 AM UTC

Hi @NSemrHomeInit​ ,

Which version of CubeMX are you using ?

Can you please check with the latest version of CubeMX and CubeIDE?

Thanks, Khouloud

NSemrHomeInit
Associate III
Dec 8, 2020 12:32 PM UTC

Hello Khouloud,

I am using the CubeMx 5.6.1 and CubeIDE 1.5.0. Could you confirm please that I am using the latest version?

My RTOS is running on this version of CubeIDE but have an issue.

  1. I am using TIM1 for RTOS ==> OK (task 1)
  2. I am using TIM3 to blink an Led and to handle an interrupt using FreeRTOS ==> NOK (task2)

I could understand why the TIM3 interrupt is not triggered? Could you please help to solve this?

The tim3 global interrupt is enabled and the preemption priority is 5. My RTOS configuration for the RTOS header file are:

Library_lovest_interrrupt_priority = 15

Library_max_syscall_interrupt_priority = 5

I am adding this call function HAL_NVIC_SetPriorityGrouping (NVIC_PRIORITYGROUP_4); but nothing changed, still have the same problem.

Thanks in advance,

S.Tarik

Khouloud ZEMMELI
ST Employee
Dec 8, 2020 1:43 PM UTC

Hi @NSemrHomeInit​ 

The Latest CubeMX version is 6.1.0, please check if you still find compilation error with the default project.

Thanks, Khouloud