Skip to main content
cxiao
Associate
Mar 12, 2019 1:42 AM UTC
Question

Maximum APB clock frequency on STM32H743 family

Hi,

What is the maximum frequency that the APB buses on the STM32H743 can be run at?

In CubeMX's Clock Configuration page when trying to configure the APB bus frequencies, there is a note on the APB clock that its maximum frequency is 100MHz. CubeMX also enforces this constraint and will not allow me to set the bus frequency on any APB to more than 100MHz. However, I can't find any information about this anywhere in the reference manual, nor the datasheet, so I am not sure what the maximum frequency actually is.

0690X0000087nULQAY.png

I am aware that it is possible to run the timer peripherals which use the APB clock as a clock source at a higher frequency than the APB clock, but I would like to know what the maximum bus frequency of the APB itself is.

Best,

Cindy

This topic has been closed for replies.

3 replies

Tesla DeLorean
Guru
Mar 12, 2019 4:51 AM UTC
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
cxiao
cxiaoAuthor
Associate
Mar 13, 2019 12:54 AM UTC

Thanks! Datasheet fatigue definitely got the best of me there.

Khouloud ZEMMELI
ST Employee
Mar 12, 2019 7:51 AM UTC

Hello @cxiao​ 

Concerning the​ APB Peripheral Clock , the maximum frequency is 100 MHz as it's indicated in CubeMX , and for the APB Timer Clock the maximum frequency is 200 MHz.

Best Regards,

Khouloud.