Skip to main content
JRS
Associate III
Nov 14, 2019 8:12 AM UTC
Question

lwip update to current version

Hi,

regarding the lwip stack in cube-mx (currently 5.4) the version is fixed at 2.0.3 .

Is there a plan to move on to the current version 2.1.2 of the stack?

If not, are there any known pitfalls, when manually migrating the underlying stack to another version? (-> where can I find Info on what is CubeMX-specific?)

Best regards,

Jan

This topic has been closed for replies.

5 replies

waclawek.jan
Super User
Nov 14, 2019 8:25 AM UTC

Hi Jan,

It's exactly your question (possible pitfalls, so somebody must go and discover them all - and who knows, where all the bugs potentially revealed by the vast user base, lie) which makes using newer version of the 3rd party libraries impractical for CubeMX - it potentially breaks existing users code, with a subsequent wave of complaints. Updates are plague, not advancement.

So, you should probably go and find out yourself, perhaps starting with getting the stock 2.0.3 and comparing it to the cubeMX one.

What is it in the current lwip you really need and is not in the older one?

JW

PS. Please change your username to a normal nick.

JRS
JRSAuthor
Associate III
Nov 14, 2019 8:33 AM UTC

I did compare the 2.03 versions. I found little changes in the http area.

Like in httpd.c:

#if LWIP_HTTPD_TIMING
#include "lwip/sys.h"
#endif

However in 2.0.3 to 2.1.2 a lot has changed. So I will have to go through the options manually.

I need the JSON SSI support with Json-tags, which was added then.

Best regards,

Jan

waclawek.jan
Super User
Nov 14, 2019 8:45 AM UTC

> I need the JSON SSI support with Json-tags, which was added then.

I see.

Isn't this constrained to the http part? Isn't that sort of a separate "helper" project? (It was so in lwip 1.4 I am still using). If it's so, it should have a relatively constrained impact.

JW

JRS
JRSAuthor
Associate III
Nov 14, 2019 8:58 AM UTC

At the basic you have to add .json in the struct of ssi compliant extensions and change the way the Tags are found. There have however been some more basic changes in how this is done in the new stack.

Khouloud ZEMMELI
ST Employee
Nov 21, 2019 8:41 AM UTC

​Hello @JRS​ 

Yes, this lwip version will be integrated in cubeMX in the future.

Best Rgerads,

Khouloud.