PTihaAssociate III6 years agoJul 23, 2020 2:10 PM UTCQuestionLwIP raw api with static IP and NUCLEO-F429ZI slow startup: It takes 15 seconds for the first ping.4 replies1548 viewsHello!I created a standard LwIP NO-OS project with static IP. Everything works perfectly, but it takes ~ 15 seconds for the first PING response.After that the ping times ~1.4 ms.I tried what happens when I disconnect the Ethernet cable and then reconnect it.It took another 15 seconds to re-establish the connection (the first ping response arrived).The MCU core clock is 168 MHz. SysTick is 1ms.Why can this be?NUCLEO-F429ZI.ioclwip.cSTM32CubeIDESTM32CubeMXEthernet