Skip to main content
Senior
March 8, 2025
Question

LTDC Window Horizontal Stop and Vertical Stop: 800 or 799?

Hi,

when configuring the LTDC for a 800 x 800 display, the Window Horizontal Start is by default set to 0 which suggests it is a 0-indexed range. So do you set the Window Horizontal Stop and Window Vertical Stop to 800 or to 799?

 

As a separate question, if you use TouchGFX, are those values changed according to what you put on various pages and/or by some settings there?

 

Thank you :)

Rick

Ricko_0-1741475158336.png

 

This topic has been closed for replies.

2 replies

INaee.1
Associate II
March 10, 2025

Hi @Ricko 

the vertical and horizontal stop should be 800 not 799.
I have played a lot with TouchGFX and always used like this .

here is one of my latest experiment with Google Nexus 7 inch display with 1280x800 resolution. 

 

WhatsApp Image 2025-01-30 at 11.28.09_177f402c.jpg

WhatsApp Image 2025-02-02 at 23.29.36_12a05473.jpg

The first screen is connected with ComAp's Inteli-compact NT over modbus RTU and my screen has more then 30 parameters , updating in real time. also the icons are changing colors as I programmed.

Here is TouchGFX running on Samsung Tab3 10.1" 1280x800 TFT. (STM32H745)

WhatsApp Image 2023-08-02 at 10.43.54.jpg

Here is TouchGFX running on Samsung Tab3 7" 1024x600 TFT. (STM32H745)

_legacyfs_online_stmicro_images_0693W00000dDSgCQAW.png

My custom designed board is similar as below.

20230811_104211.jpg

If you need some guidance then don't hesitate.
regards
I.N

RickoAuthor
Senior
March 10, 2025

That answers that question. Thank you @INaee.1 

I will let you know if I do. Thank you, much appreciated :)