Skip to main content
NickO
Associate III
December 2, 2025
Solved

Linker Errors when enabling CMSIS RTOS v2 and TrustZone

I have started a new project using STM32H573. This is using the following:

  • Cube MX 6.16
  • Cube IDE 2.0 - Build: 26820_20251114_1348 (UTC)

The project has secure zone enabled. I have written bare metal code and shown I can run/debug code in the non-secure environment without issues, and I can invoke non-secure callable functions etc.

My problem comes when I add Free RTOS and enable CMSIS RTOS v2 to the non-secure side.

When I build, I get linker errors (see below).

When I search the forums, there have been similar issues raised, but most are quite old posts or seem overly complex (which always worries me)

``

C:/Users/531023/git/TEML20/Monitor/NonSecure/Debug/../Core/Src/app_freertos.c:86:(.text.MX_FREERTOS_Init+0xa): undefined reference to `osThreadNew'
C:/ST/STM32CubeIDE_1.18.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.100.202509120712/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/bin/ld.exe: ./Core/Src/app_freertos.o: in function `StartDefaultTask':
C:/Users/531023/git/TEML20/Monitor/NonSecure/Debug/../Core/Src/app_freertos.c:110:(.text.StartDefaultTask+0xa): undefined reference to `osDelay'
C:/ST/STM32CubeIDE_1.18.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.100.202509120712/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/bin/ld.exe: ./Core/Src/main.o: in function `main':
C:/Users/531023/git/TEML20/Monitor/NonSecure/Debug/../Core/Src/main.c:96:(.text.main+0x10): undefined reference to `osKernelInitialize'
C:/ST/STM32CubeIDE_1.18.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.100.202509120712/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/Users/531023/git/TEML20/Monitor/NonSecure/Debug/../Core/Src/main.c:101:(.text.main+0x18): undefined reference to `osKernelStart'
collect2.exe: error: ld returned 1 exit status
make: *** [makefile:91: Monitor_NonSecure.elf] Error 1
"make -j16 all" terminated with exit code 2. Build might be incomplete.

 I also get the following warning (which is likely related):

Invalid project path: Missing project folder or file: \Monitor_NonSecure\RTOS2 for Source path. Monitor_NonSecure pathentry Path Entry Problem

 

Souhaib MAZHOUDBest answer
ST Technical Moderator
December 2, 2025

Hello @NickO 

Yes, the compilation error you are facing are caused by the fact that X-Cube-FREERTOS is not selected for the secure project. Therefore, some dependencies are not generated and will lead to those errors.

To give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

7 replies

NickO
NickOAuthor
Associate III
December 2, 2025

Now I am getting this (and I don't know what I changed):

C:/Users/531023/git/TEML20/Monitor/Middlewares/Third_Party/FreeRTOS/Source/portable/GCC/ARM_CM33/non_secure/port.c:1133:(.text.vPortSVCHandler_C+0x38): undefined reference to `SecureContext_AllocateContext'
C:/ST/STM32CubeIDE_1.18.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.100.202509120712/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/Users/531023/git/TEML20/Monitor/Middlewares/Third_Party/FreeRTOS/Source/portable/GCC/ARM_CM33/non_secure/port.c:1138:(.text.vPortSVCHandler_C+0x5e): undefined reference to `SecureContext_LoadContext'
C:/ST/STM32CubeIDE_1.18.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.100.202509120712/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/Users/531023/git/TEML20/Monitor/Middlewares/Third_Party/FreeRTOS/Source/portable/GCC/ARM_CM33/non_secure/port.c:1149:(.text.vPortSVCHandler_C+0x76): undefined reference to `SecureContext_FreeContext'
C:/ST/STM32CubeIDE_1.18.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.100.202509120712/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/Users/531023/git/TEML20/Monitor/Middlewares/Third_Party/FreeRTOS/Source/portable/GCC/ARM_CM33/non_secure/port.c:1158:(.text.vPortSVCHandler_C+0x7c): undefined reference to `SecureInit_DePrioritizeNSExceptions'
C:/ST/STM32CubeIDE_1.18.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.100.202509120712/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/Users/531023/git/TEML20/Monitor/Middlewares/Third_Party/FreeRTOS/Source/portable/GCC/ARM_CM33/non_secure/port.c:1161:(.text.vPortSVCHandler_C+0x80): undefined reference to `SecureContext_Init'
C:/ST/STM32CubeIDE_1.18.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.100.202509120712/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/bin/ld.exe: ./Middlewares/RTOS2/CMSIS/RTOS2/Core/TZ_Non_Secure/portasm.o: in function `PendSV_Handler':
C:/Users/531023/git/TEML20/Monitor/Middlewares/Third_Party/FreeRTOS/Source/portable/GCC/ARM_CM33/non_secure/portasm.c:433:(.text.PendSV_Handler+0x10): undefined reference to `SecureContext_SaveContext'
C:/ST/STM32CubeIDE_1.18.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.100.202509120712/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/Users/531023/git/TEML20/Monitor/Middlewares/Third_Party/FreeRTOS/Source/portable/GCC/ARM_CM33/non_secure/portasm.c:433:(.text.PendSV_Handler+0x5e): undefined reference to `SecureContext_LoadContext'
collect2.exe: error: ld returned 1 exit status
make: *** [makefile:94: Monitor_NonSecure.elf] Error 1

 

 

ST Technical Moderator
December 2, 2025

Hello @NickO 

Could you please attach your ioc, in order to further investigate the issue?

KR, Souhaib

To give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
NickO
NickOAuthor
Associate III
December 2, 2025

Thank you for replying. Please see attached.