Skip to main content
one V
Associate III
Dec 7, 2021 7:30 AM UTC
Question

It is strongly recommended that ST specifically generate a Callback.c file when Cubemx generates the Keil project, and all the callback functions that actually need to be used can be put into the Callback.c file.

..

This topic has been closed for replies.

1 reply

Sara BEN HADJ YAHYA
ST Technical Moderator
Dec 29, 2021 9:41 AM UTC

Hello @one V​ ,

STM32CubeMX allows the configuration of STM32 microcontrollers and microprocessors, as well as the generation of the corresponding initialization code. The callback functions are not always needed but when they are, the user can add them manually in main.c file.

Anyways, I'll raise your request internally to be reviewed and to see how we can address a modification.

If you issue is solved, please close this post by clicking the "Select as Best" button. This will help other members of the community find this response more quickly :)

Thanks for your contribution,

Sara.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.