Issue setting clocks on STM32L412 IDE 1.4.2
Hi,
I was playing around a bit with the clocks.
I had it set up to run on 48MHz from MSI.
I then choose PLL on 64MHz but couldn't get the 1µs timer pulse I wanted (prescaler on 63 for TIM2 got me something about 1,178µs)
I then wanted to get back to MSI, but configuration tool found an issue with RCC
Flash latency is marked as a problem with 3 waitstates.
I can do nothing about it since its greyed out
any idea how I can get back to 48MHz MSI
cheers,
Bob