Skip to main content
Jeremi Wójcicki
Associate II
Feb 6, 2017 10:00 AM UTC
Question

Is there going to be C++ support in the future CubeMX releases?

Posted on February 06, 2017 at 11:00

I would like to know if guys from ST are planning to support C++ in the next releases of the CubeMX? I know that you can port your project, but it's not hassle free operation, especially if you often regenerate your project through CubeMX (e.g. by adding some peripherals, changing configuration etc. etc.). I would really apprecciate it!

#support #cubemx #c++
This topic has been closed for replies.

6 replies

ST Technical Moderator
Feb 6, 2017 10:31 AM UTC
Posted on February 06, 2017 at 11:31

Hello

jeremi.wojcicki

‌,

You request is reported internallyfor more investigation.

Your comments and suggestions are welcome to improve our solutions.

Best Regards

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Jeanne Joly
Associate
Jan 18, 2018 2:25 PM UTC
Posted on January 18, 2018 at 15:25

Hi

Wojcicki.Jeremi

,

We do understand the need for you to generate C++project and this need is well known internally.

However, for the moment, with the success of STM32CubeMX, we have a lot of requests/suggestions to study andmanyimprovements to integrate.

And the C++ generation project item is not yet under study currently.

Sorry, for the inconvenience it may cause.

BR. Jeanne

snigg
Associate III
Oct 29, 2018 9:51 PM UTC

Please understand that this really is an inconvenience! I urge ST to reconsider. The code that is generated does need a lot of cleaning to use it in a productive environment. Yet coding by hand is too time consuming and error prone.

HJafa.1
Visitor II
Dec 18, 2019 8:43 PM UTC

Hi, I was looking for the solution to use CPP codes inside STM32CubeMX IDE . I came to an solution which I published on this small step by step tutorial .

Hope this would be helpful to others as well.

sarp daltaban
Associate II
Apr 3, 2020 6:51 PM UTC

I'd be a volunteer to support C++ integration within FreeRTOS and LwIP. Please take this under study.

Fzefz.1
Visitor II
Jul 16, 2021 1:39 PM UTC

Heya,

Can you at leat support .cpp main file via an optionnal checkbox ?

It's anoying to rename main.cpp to main.c everytime i regenerate the config. (i use cubeMX main template)

It would be very simple to implement (if any main.c search for main.cpp and use it like if it was main.c).

That would be very convenient.

Best regards