Question
Is there a way to specify that a given timer channel needs to use a 5V tolerant pin (FT)?
I am using an STM32G4 and working in STM32CubeIDE with the MX interface.
The software is great about assigning pins to allow for all of my functionality but I do not see a way to specify this. I am using TIM 1,3,4,8 for encoder counting with CH1&2 on each. I want to be able to handle 5V and 3.3V quadrature encoders on these encoder counting timers. They all have 5V tolerant (FT) pin options but the default selections are not always the FT option. Any ideas on how to have the software do the pin selection in this way would be appreciated!
Thanks :)