Skip to main content
ASter.1
Associate
Sep 20, 2021 8:46 AM UTC
Question

Is there a way to create a STM32CubeMX project from a STM32CubeIDE example?

Hello All,

I have an STM32WB55 Nucleo board and I want to use the BLE_HID example from the FW folder 1.12.1. I have successfully built, uploaded, and ran the example on my board, however, I am now running into 2 problems:

  • If I try to copy the BLE_HID folder and paste is somewhere other than:

"/Users/<username>/STM32Cube/Repository/STM32Cube_FW_WB_V1.12.1/Projects/P-NUCLEO-WB55.Nucleo/Applications/BLE/BLE_Hid"

the STM32CubeIDE will throw the error:

make: *** No rule to make target '/Utilities/lpm/tiny_lpm/stm32_lpm.c', needed by 'Utilities/stm32_lpm.o'. Stop.

And will not build. How do I overcome this problem?

  • The BLE HID functionality is only a part of my final product, and I want to build my project starting from the example but I want to be able to use the CubeMX program. Is there a way to take the example and turn it into a CubeMX project?

Any help is appreciated!

Almog

This topic has been closed for replies.

1 reply

Mike_ST
ST Technical Moderator
Sep 20, 2021 11:46 AM UTC

1) The BLE_HID Folder is not the only part of the project:

Each project in the firmware package compiles others folders like :

Users/<username>/STM32Cube/Repository/STM32Cube_FW_WB_V1.12.1/Utilities

Users/<username>/STM32Cube/Repository/STM32Cube_FW_WB_V1.12.1/Drivers/BSP/P-NUCLEO-WB55.Nucleo

Users/<username>/STM32Cube/Repository/STM32Cube_FW_WB_V1.12.1/Drivers/CMSIS

Users/<username>/STM32Cube/Repository/STM32Cube_FW_WB_V1.12.1/Drivers/STM32WBxx_HAL_Driver

Users/<username>/STM32Cube/Repository/STM32Cube_FW_WB_V1.12.1/Middlewares

So,

-   either you restructure the project,

-   either you just copy the entire STM32Cube_FW_WB_V1.12.1 folder, all Projects excluding the BLE_Hid one

and delete the uneeded folders in Users/<username>/STM32Cube/Repository/STM32Cube_FW_WB_V1.12.1/Drivers/BSP/

2) Unless there is an .ioc file, there is no automatic tool to do that. Everything would be manual.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.