Skip to main content
Jul 28, 2022 4:52 AM UTC
Question

Is Cubemx ethernet reworked?

Hello friends,

I used to use stm32cubemx ethernet with previous versions of cubemx and cubeide. However, the new release wondered me in the way that it didn't generate any code for the ethernet peripheral initialization, by which I mean formerly there was a function in the generated code "MX_ETH_init()". But in the recent version even with the activation of LWIP this function isn't generated. I use stm32f429bit6 chip along with stm32cubemx 6.1.1 and cubeide 1.10.1.

Moreover, there was Phy Address Parameter in parameter settings in previous versions which I couldn't find that in the new release.

This topic has been closed for replies.