Skip to main content
JTari
Visitor II
Oct 19, 2019 3:08 AM UTC
Question

Is CubeMX config generating an overrun error when using ADC peripheral with DMA ?

I'm using an STM32F446RE nucleo-64 board with STM32CubeIDE.

I was testing a potentiometer and noticed that the default code generated by cubeMX leads to an overrun error in the ADC peripheral. The issue can be manually solved by calling MX_DMA_Init() before MX_ADC1_Init() in main.c.

To reproduce the issue, my configuration on the CubeMX interface is as follows:

  • ADC1_channel0 enabled.
  • DMA2 stream 0 in peripheral to memory, circular mode.
  • DMA and continous mode enabled.
  • Only 1 regular conversion.
  • sampling time of 480 cycles per conversion.

In main(), the regular conversion is triggered by HAL_DMA_START() just before the while loop.

This works as expected :

int main(void)
{
 HAL_Init();
 
 SystemClock_Config();
 
 MX_GPIO_Init();
 MX_USART2_UART_Init();
 MX_DMA_Init(); // Has been moved manually before MX_ADC1_Init();
 MX_ADC1_Init();
 
 if (HAL_ADC_Start_DMA(&hadc1, g_raw_adc_reading, BUFLENGTH) != HAL_OK)
	 Error_Handler();
 while (1)
 {
 }
}

But if line 9 & 10 are inverted, as generated by cubeMX, the overrun flag will be set in the ADC1 status register. Unless I am missing something on the HAL library.

This topic has been closed for replies.

2 replies

waclawek.jan
Super User
Oct 19, 2019 7:33 AM UTC

Yes, it appears to be an error.

JW

MChev.1
Visitor II
Nov 25, 2021 11:25 AM UTC

Yes, there's a problem in CubeMX. It has been 2years and still the issue persists!