Skip to main content
EdgyAI
Associate II
December 1, 2023
Question

Invalid SRAM6 Warning for U5A5ZJT6Q

Operating System: Windows 10

STM32CubeMX version: 6.10.0

STM32CubeU5 Firmware Package V1.4.0 / 20-October-2023

When I attempt to validate my X-CUBE-AI model on target, I receive the following pop-up:

EdgyAI_0-1701470114151.png

Exploring STM32CubeMX.log shows the following warning:

[WARN] IP:2119 - SRAM6PowerDownInRunMode not found: check if there is a RefParameter without a condition.

The U5A5 doesn't even have an SRAM6, if I am reading the datasheet correctly.  When I look at the configuration options in CubeMX, I can't see anything for SRAM6 in the PWR section.

This topic has been closed for replies.

3 replies

ST Technical Moderator
December 4, 2023

Hello @EdgyAI, 

Thank you for having reported the point.

Can you please share your ioc and log files for deep check.

I escalated this internally to CubeMx team in an internal ticket (ID 167860) to take a closer look at this issue.

(PS: ID 167860, is an internal tracking number and is not accessible or usable by customers).

Imen

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
EdgyAI
EdgyAIAuthor
Associate II
December 4, 2023

Imen,

Please see attached files.  When I try to upload my .ioc file, I receive the following error:

The attachment's nucleo-u5a5zj-q.ioc content type (application/octet-stream) does not match its file extension and has been removed.

To get around this, I simply renamed it as the .txt file below.

I should also note that if I ignore the code generation error and proceed, validation on target executes successfully.

Thank you.

ST Technical Moderator
August 1, 2025

Hello @EdgyAI ,

This issue is fixed in the latest release of STM32CubeMx v6.15.

Thank you for your contribution.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks