Skip to main content
Associate II
January 25, 2026
Question

Incorrect SAU Configuration From MMT on STM32H573 with Backup RAM Enabled

When using the memory management tool (MMT) on the STM32H573 to set the backup RAM as secure it generates an invalid secure attribution unit (SAU) config:

#define SAU_INIT_REGION5 1
#define SAU_INIT_START5 0x40000000 /* start address of SAU region 5 */
#define SAU_INIT_END5 0x400373FF /* end address of SAU region 5 */
#define SAU_INIT_NSC5 0

The above code is the last region the MMT defines for the SAU.

Typically the tool would define the region 0x40000000 to 0x4fffffff (the non-secure peripheral address space) as non-secure. However 0x40036400 is the start of the backup RAM address space which shouldn't be made non-secure.

Since this is the last SAU region, there is nothing configuring the region 0x40037400 to 0x4fffffff as non-secure, and so hard faults occur when e.g. trying to access the non-secure RCC address space.

I believe correctly generated code should look like the below:

#define SAU_INIT_REGION5 1
#define SAU_INIT_START5 0x40000000 /* start address of SAU region 5 */
#define SAU_INIT_END5 0x400363FF /* end address of SAU region 5 */
#define SAU_INIT_NSC5 0

#define SAU_INIT_REGION6 1
#define SAU_INIT_START6 0x40037400 /* start address of SAU region 6 */
#define SAU_INIT_END6 0x4FFFFFFF /* end address of SAU region 6 */
#define SAU_INIT_NSC6 0

Please can the MMT be updated to patch this? 

5 replies

ST Technical Moderator
January 26, 2026

Hello @ben5050 

Let me thank you for your post.

For more investigation, could you please provide your IOC.File.

Thanks

Mahmoud 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
ben5050Author
Associate II
January 26, 2026

Hi Mahmoud,

I've attached the IOC file.

Kind regards,

Ben

ST Technical Moderator
January 26, 2026

Hello @ben5050 ,

 

After checking internally, the SAU configuration generated by the Memory Management Tool is correct and expected.

When Backup RAM is secure on STM32H573, CubeMX intentionally ends the non-secure peripheral SAU region before the Backup RAM start address.

As a result, the non-secure SAU region is limited to 0x40000000-0x400363FF and the remaining address space is not automatically configured as non-secure, in accordance with Trust Zone security model.

Any additional non-secure peripheral regions must be explicitly defined by the user if required.

 

Thanks

Mahmoud

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.