Skip to main content
Associate
July 15, 2025
Question

Inconsistent on STM32N657A0 between Datasheet and CubeMX 6.15.0 configuration

Hi,

I got the problem on choosing FMC pin definition of STM32N657A0 in CubeMX 6.15.0. As the datasheet said the FMC_NORMUX is supported by the chip, I cannot find corresponding settings in CubeMX as the screenshots.

Thanks.

Screenshot 2025-07-15 at 10.04.31 PM.png

Screenshot 2025-07-15 at 10.32.51 PM.pngScreenshot 2025-07-15 at 10.05.00 PM.png

This topic has been closed for replies.

3 replies

TDK
July 15, 2025

Probably the chip package doesn't have all pins necessary for that interface, so it doesn't support configuring any of them.

Enable the interface in the FMC tab rather than pin by pin. If it's not there, probably necessary pins are missing.

"If you feel a post has answered your question, please click ""Accept as Solution""."
ldxAuthor
Associate
July 16, 2025

Thanks for getting in touch! Unfortunately, there’s no FMC tab under this chip in CubeMX. I’m a bit confused because the datasheet mentions that it supports FMC_NORMUX. Could you help me understand how to configure it? I’m wondering if it’s a bug in CubeMX or if I’m just setting it up incorrectly.

KDJEM.1
ST Technical Moderator
July 16, 2025

Hello @ldx and welcome to the community,

 

Thank you for bringing this issue to our attention.

I reported the issue internally for checking.

Internal ticket number: 214197 (This is an internal tracking number and is not accessible or usable by customers).

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.