Skip to main content
AShah.10
Visitor II
Nov 23, 2022 2:46 PM UTC
Question

If I want to make custom code structure or if I want to maintain 2 applications which have 2 different folders but can use same STM code, Is it possible? Can I change directory structure from cube MX or from any other tool?

If I want to make custom code structure or if I want to maintain 2 applications which have 2 different folders but can use same STM code, Is it possible? Can I change directory structure from cube MX or from any other tool? Like 2 applications which have different .project file, but using same STM resources like RTOS. Want to add new folders as well

This topic has been closed for replies.

1 reply

Pavel A.
Nov 23, 2022 9:05 PM UTC

> If I want to make custom code structure or if I want to maintain 2 applications which have 2 different folders but can use same STM code, Is it possible?

Yes, entirely possible.

> Can I change directory structure from cube MX or from any other tool?

No, AFAIK the CubeMX (or the CubeIDE plugin) are not that flexible.

But one can tweak the [generated] eclipse project in various ways.