Skip to main content
Abdelmalek BELLOULA
Associate III
May 29, 2022 7:11 AM UTC
Question

If I activate the LSE for the RTC instead of the LCI, using version 6.4 of stm32cubemx , the "SystemClock_Config()" function generates an error. is there a solution to solve the problem using version 6.4 of stm32cubemx.

Initially I used version 6.5 of stm32cubemx to generate my project for stm32h743 and as I use the ADC module which I cannot get to work with this version, I switched to version 6.4, I So the problem of the ADC is solved, it works very well except that If I activate the LSE for the RTC instead of the LCI, using version 6.4 of stm32cubemx , the "SystemClock_Config()" function generates an error. 

This topic has been closed for replies.