Skip to main content
goobinooz
Associate II
Oct 10, 2022 8:33 AM UTC
Question

I want know how configure two interfaces hid for stm32 / cube MX

hi,

I need to have a code example for understand how have a keyboard and mouse in one project, can you help me please!

This topic has been closed for replies.

4 replies

ST Technical Moderator
Oct 10, 2022 7:56 PM UTC

Hello @goobinooz​ and welcome to the Community :)

Which device are you using?

I advise you to check the HID example within STM32Cube MCU package relevant to your device.

Have a look at these resources:

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
goobinooz
goobinoozAuthor
Associate II
Oct 10, 2022 8:12 PM UTC

I use STM32F103C8Tx but your example refer to one interface but me I want two interface and the training not responding to my needed, I want emulate a mouse + a keyboard in my code

Tesla DeLorean
Guru
Oct 10, 2022 8:59 PM UTC

https://community.st.com/s/question/0D50X0000Az4FiiSQE/how-can-i-implement-multiple-usb-hid-devices-on-stm32f042-or-stm32f103

You'd need to create a CONFIGURATION descriptor describing ALL the HID devices you want

A "Composite" device would be one offering more than one class. That would use a INTERFACE descriptor

On a MSC Class device you'd allow for multiple LUN (Logical Unit Number), and the OS could then Inquire the nature of each, ie name, size (sector, capacity), type (optical, magnetic, etc), using standard SCSI/ATAPI type command set.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
goobinooz
goobinoozAuthor
Associate II
Oct 10, 2022 9:09 PM UTC

can I have a exemple of code because my competences are so limited