Skip to main content
jdowdster
Associate II
Sep 25, 2020 1:12 PM UTC
Solved

I'm using a STM32F746-Discovery kit and the development is being done on a linux PC using Trustudio 9.3.0. Watchdog is going off and I can't connect to reprogram

As mentioned above I can't connect as the watchdog is continuously going off. I used the STM32CubeMx to enable the IWDG and it created the s/w load which enables the IWDG but doesn't refresh it. I know how to fix it in the s/w but my debugger under TrueStudio won't connect to load the new image. My board is continuously resetting.

Have I bricked my board or is there some s/w tool I can use to erase the board? Remember I am running on linux.

Thanks in Advance for any help.

Cheers!!

This topic has been closed for replies.
KnarfB
KnarfBBest answer
Super User
Sep 25, 2020 8:17 PM UTC

If you enabled the IWDG hardware start, this can be disabled by using the STM32CubeProgrammer by setting some option bytes (OB).

1 reply

KnarfB
KnarfBBest answer
Super User
Sep 25, 2020 8:17 PM UTC

If you enabled the IWDG hardware start, this can be disabled by using the STM32CubeProgrammer by setting some option bytes (OB).