Skip to main content
raffin
Associate III
Jan 13, 2020 10:11 AM UTC
Question

I have to implement an HTTP client on a STM32F4 MCU. According to Table 2 in RN0044 (and LWIP docs), the httpclient should be part of LWIP but when I generate my code, I am not able to get it. Is there some option to check in CubeMX configuration?

 I noticed that cubeMX uses the LWIP 2.0.3 while the latest LWIP release is the 2.1.0.

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
Jan 13, 2020 11:27 AM UTC

ST tends to be behind the curve updating middleware.

​

That said LWIP has surely had working HTTP examples for literally years.

​

Perhaps look at the HAL examples rather that let CubeMX prepare you a fresh bowl of dogfood for breakfast​.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
raffin
raffinAuthor
Associate III
Jan 13, 2020 12:08 PM UTC

Thank you for the answer Clive1,

as far as I am concerned, the HAL examples involve only HTTP servers which exploit the "fresh bowl of dogfood" httpd, provided by LWIP. In principle the LWIP provides also some code for an http client but it is not included in the output of the Cube. At this point I think the best strategy could be to merge the Cube LWIP ver 2.0.3 with the current stable release 2.1.0 of LWIP to get the missing package "HTTP client" in the app section.