Skip to main content
EPate.1
Associate
Feb 11, 2021 11:42 AM UTC
Solved

I have a Discovery 32F412ZGT6 dev board and I'm trying to use the FSMC peripheral. The ioc file assigns pins PC11 and PC12 to D2 & D3 respectively. These pins are not available on the pin headers on the board and I cannot re-assign them.

So MX assigns the following pins for FSMC

NWE -> PC2

NOE -> PC5

NE1 -> PD7

RST -> PD11

FMC addr A18 - PD13

D0 -> PB14

D1 -> PD15

D2 -> PC11 (Assigned to micro sd card)

D3 -> PC12 (Assigned of micro sd card)

D4 -> PA2

D5 -> PA3

D6 -> PA4

D7 -> PA5

Can you help with how I get access to PC11 and PC12?

Thank you!

This topic has been closed for replies.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Feb 11, 2021 12:14 PM UTC

Well, this is the DISCOVERY board, which is similar to the EVALUATION boards to demonstrate the functionality of the specific controller and possibly be used to create your own system. Some of the DISCOVERY kits have a few free pins which can be used for some tests. However, you need to find them using the schematics and documentation. In most cases it is too difficult to reassign used pins.

Perhaps you should consider the NUCLEO boards if you are starting your own development and want to have (almost) full freedom in using the available pins and peripherals.

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Good luck!

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

2 replies

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Feb 11, 2021 12:14 PM UTC

Well, this is the DISCOVERY board, which is similar to the EVALUATION boards to demonstrate the functionality of the specific controller and possibly be used to create your own system. Some of the DISCOVERY kits have a few free pins which can be used for some tests. However, you need to find them using the schematics and documentation. In most cases it is too difficult to reassign used pins.

Perhaps you should consider the NUCLEO boards if you are starting your own development and want to have (almost) full freedom in using the available pins and peripherals.

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Good luck!

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
EPate.1
EPate.1Author
Associate
Feb 11, 2021 4:28 PM UTC

Great!

Thank you for your fast reply!

I will look at a Nucleo board with FSMC

Regards,

Eric