Skip to main content
KSmel.1
Associate
May 20, 2022
Solved

I get an empty Error Message when migrating my project from CubeMX v6.2.0 FW_F7 V1.16.1 to V6.5.0 FW_F7 V1.16.2

  • May 20, 2022
  • 6 replies
  • 2364 views

I have attached the .IOC file that will not migrate. Any help would be great.

This topic has been closed for replies.
Best answer by Sara BEN HADJ YAHYA

Hello @KSmel.1​ ,

Thanks for your feedback,

The issue seems to come from a bug found in v6.5.0. We discovered that by mapping SPI3_MISO signal on PB4, JTAG (4 pins) becomes disabled where it shouldn't since JTAG (4 pins) mode does not use SYS_JTRST which can be mapped on PB4 and this latter is related to JTAG (5 pins) mode.

This issue unfortunately affected project migration to v6.5.0 however it is possible to migrate to v6.4.0 or 6.3.0.

To migrate your project to v6.5.0, I would suggest to replace JTAG (4 pins) debug mode with Serial Wire debug mode. To do so you need to open your ioc file with a text editor and you need to delete the following lines:

PB3.GPIOParameters=GPIO_Label
PB3.GPIO_Label=PB3[SWO]
PB3.Locked=true
PB3.Mode=JTAG_4_pins
PB3.Signal=SYS_JTDO-SWO
PA15.GPIOParameters=GPIO_Label
PA15.GPIO_Label=PA15[SYS_JTDI]
PA15.Locked=true
PA15.Mode=JTAG_4_pins
PA15.Signal=SYS_JTDI

By deleting those lines, PB3 and PA15 will get back to their reset state and SYS_JTDO-SWO and SYS_JTD will no longer be used. So only SYS_JTMS-SWDIO and SYS_JTCK-SWCLK signals will be left for debug, these signals represent the serial wire debug mode.

After the delete, you need to save the ioc file and than open it with v6.5.0 to migrate your project.

Mapping SPI3_MISO signal on PC11 would be another option but in your case I think it is not since you are using QUADSPI (Bank2 with Quad SPI lines) and it requires QUADQPI_BK2_NCS signal which can be mapped only on PC11.

With this being said, I submitted an internal ticket to solve this issue. I will keep you posted.

Internal ticket number: 129210 (This is an internal tracking number and is not accessible or usable by customers).

I hope this helps and if you have further question, do not hesitate to get back to me :smiling_face_with_smiling_eyes:

If your issue is solved, please close this post by clicking the "Select as Best" button. This will help other members of the community find this response more quickly :)

Sara.

6 replies

Sara BEN HADJ YAHYA
ST Technical Moderator
May 24, 2022

Hello @KSmel.1​ ,

Thanks for your feedback,

The issue seems to come from a bug found in v6.5.0. We discovered that by mapping SPI3_MISO signal on PB4, JTAG (4 pins) becomes disabled where it shouldn't since JTAG (4 pins) mode does not use SYS_JTRST which can be mapped on PB4 and this latter is related to JTAG (5 pins) mode.

This issue unfortunately affected project migration to v6.5.0 however it is possible to migrate to v6.4.0 or 6.3.0.

To migrate your project to v6.5.0, I would suggest to replace JTAG (4 pins) debug mode with Serial Wire debug mode. To do so you need to open your ioc file with a text editor and you need to delete the following lines:

PB3.GPIOParameters=GPIO_Label
PB3.GPIO_Label=PB3[SWO]
PB3.Locked=true
PB3.Mode=JTAG_4_pins
PB3.Signal=SYS_JTDO-SWO
PA15.GPIOParameters=GPIO_Label
PA15.GPIO_Label=PA15[SYS_JTDI]
PA15.Locked=true
PA15.Mode=JTAG_4_pins
PA15.Signal=SYS_JTDI

By deleting those lines, PB3 and PA15 will get back to their reset state and SYS_JTDO-SWO and SYS_JTD will no longer be used. So only SYS_JTMS-SWDIO and SYS_JTCK-SWCLK signals will be left for debug, these signals represent the serial wire debug mode.

After the delete, you need to save the ioc file and than open it with v6.5.0 to migrate your project.

Mapping SPI3_MISO signal on PC11 would be another option but in your case I think it is not since you are using QUADSPI (Bank2 with Quad SPI lines) and it requires QUADQPI_BK2_NCS signal which can be mapped only on PC11.

With this being said, I submitted an internal ticket to solve this issue. I will keep you posted.

Internal ticket number: 129210 (This is an internal tracking number and is not accessible or usable by customers).

I hope this helps and if you have further question, do not hesitate to get back to me :smiling_face_with_smiling_eyes:

If your issue is solved, please close this post by clicking the "Select as Best" button. This will help other members of the community find this response more quickly :)

Sara.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
KSmel.1
KSmel.1Author
Associate
May 25, 2022

Thank you. I was able to migrate the project successfully.

Sara BEN HADJ YAHYA
ST Technical Moderator
May 27, 2022

Hello @KSmel.1​ ,

After further check, it turns out that PB4 must be free (Reset sate) when using JTAG (4 pins) otherwise the debug session gets lost. This was discovered in the previous versions and fixed in v6.5.0, for your project I would recommend you to use serial wire debug as I mentioned in my previous comment.

Sara.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
KSmel.1
KSmel.1Author
Associate
May 29, 2022

I am using SWDIO and SWCLK and SWO for debug messages.

I had the 4 bits on JTag turned on for the I-Jet Trace on a 20 pin Jtag connector. How do I enable Trace in CubeMX?

0693W00000NqouUQAR.png

Sara BEN HADJ YAHYA
ST Technical Moderator
May 30, 2022

Hello @KSmel.1​ ,

Please check section 7.3 in this AN4989 , you will find everything you are looking for.

I hope this helps :smiling_face_with_smiling_eyes: ,

Sara.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
KSmel.1
KSmel.1Author
Associate
May 30, 2022

Reading it Now. Thank-you