Skip to main content
AKapl
Visitor II
Oct 13, 2020 7:05 AM UTC
Question

I can't receive from uart3 and up on STM32F730R8

I want to use circular DMA to receive data of unknown length on 4 uarts of STM32F730R8, but I receive data just on first two of them. Transmission works and I use HAL library. Code is generated by MX configuration tool and all uarts are configured identically.

HAL_UART_Receive_DMA(&huart1,readBuffer,sizeof(readBuffer));
 HAL_UART_Receive_DMA(&huart2,debgBuffer,sizeof(debgBuffer));
 HAL_UART_Receive_DMA(&huart3,Buffer1,sizeof(Buffer1));
 HAL_UART_Receive_DMA(&huart4,Buffer2,sizeof(Buffer2));
 HAL_UART_Receive_DMA(&huart6,Buffer3,sizeof(Buffer3));
 
 HAL_UART_Transmit(&huart1, (uint8_t *)&"\nHello mr. Freeman", 18, 0xFFFF);
 HAL_UART_Transmit(&huart2, (uint8_t *)&"\nHello mr. Freeman", 18, 0xFFFF);
 HAL_UART_Transmit(&huart3, (uint8_t *)&"\nHello mr. Freeman", 18, 0xFFFF);
 HAL_UART_Transmit(&huart4, (uint8_t *)&"\nHello mr. Freeman", 18, 0xFFFF);
 HAL_UART_Transmit(&huart6, (uint8_t *)&"\nHello mr. Freeman", 18, 0xFFFF);
 /* USER CODE END 2 */
 
 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
	 for(int i = 0; i<sizeof(readBuffer); i++){
		 RX[i] = readBuffer[i];
		 if(RX[i] == 0xA5){
			 HAL_UART_Transmit(&huart1, (uint8_t *)&"\nWelcome to city 17", 19, 0xFFFF);
		 }
		 readBuffer[i] = 0;
	 }
	 for(int i = 0; i<sizeof(debgBuffer); i++){
		 dbgRX[i] = debgBuffer[i];
		 if(dbgRX[i] == 0xA5){
			 HAL_UART_Transmit(&huart2, (uint8_t *)&"\nWelcome to city 18", 19, 0xFFFF);
		 }
		 debgBuffer[i] = 0;
	 }
	 for(int i = 0; i<sizeof(Buffer1); i++){
		 RX1[i] = Buffer1[i];
		 if(RX1[i] == 0xA5){
			 HAL_UART_Transmit(&huart3, (uint8_t *)&"\nWelcome to city 19", 19, 0xFFFF);
		 }
		 Buffer1[i] = 0;
	 }
	 for(int i = 0; i<sizeof(Buffer2); i++){
		 RX2[i] = Buffer2[i];
		 if(RX2[i] == 0xA5){
			 HAL_UART_Transmit(&huart4, (uint8_t *)&"\nWelcome to city 20", 19, 0xFFFF);
		 }
		 Buffer2[i] = 0;
	 }
	 for(int i = 0; i<sizeof(Buffer3); i++){
		 RX3[i] = Buffer3[i];
		 if(RX3[i] == 0xA5){
			 HAL_UART_Transmit(&huart6, (uint8_t *)&"\nWelcome to city 21", 19, 0xFFFF);
		 }
		 Buffer3[i] = 0;
	 }
}
 
static void MX_DMA_Init(void) 
{
 
 /* DMA controller clock enable */
 __HAL_RCC_DMA2_CLK_ENABLE();
 __HAL_RCC_DMA1_CLK_ENABLE();
 
 /* DMA interrupt init */
 /* DMA1_Stream1_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(DMA1_Stream1_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(DMA1_Stream1_IRQn);
 /* DMA1_Stream2_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(DMA1_Stream2_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(DMA1_Stream2_IRQn);
 /* DMA1_Stream5_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(DMA1_Stream5_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(DMA1_Stream5_IRQn);
 /* DMA2_Stream1_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(DMA2_Stream1_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(DMA2_Stream1_IRQn);
 /* DMA2_Stream2_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(DMA2_Stream2_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(DMA2_Stream2_IRQn);
 
}

This topic has been closed for replies.

1 reply

waclawek.jan
Super User
Oct 13, 2020 9:19 AM UTC

Polled Rx works?

Read out and check/post content of relevant USART and DMA registers.

JW