Skip to main content
EFons
Associate II
Jun 10, 2019 4:40 PM UTC
Question

I can't measure properly because of the ADC timing / clock (probably)

I am using the board STM32F030R8, and I am trying to measure the voltage of two different ADC channels, one at a time. The fuction SendByte is for a multiplexer, then I have to measure some voltage, the two channels are measuring different parts of the circuit. Sometimes I get a value and sometimes it is just 0.

I was succesfull using the ADC to measure different channels before. But I was not using this function SendByte. I suppose the ADC is not synchronized with the function SendByte, because when the correspondent port of the multiplexer is not set the value in the circuit is 0.

int main(void)
{
 HAL_Init();
 
 SystemClock_Config();
 
 MX_GPIO_Init();
 MX_USART2_UART_Init();
 MX_ADC_Init();
 
 while (1)
 {
	HAL_ADC_Start(&hadc); /* Start the ADC */
 
	SendByte(0x01);
	if(HAL_ADC_PollForConversion(&hadc, 100) == HAL_OK){ /* Channel 0 */
		media_0 = HAL_ADC_GetValue(&hadc);
		v_0 = 0.0008*media_0;
	}
 
	SendByte(0x02);
	if(HAL_ADC_PollForConversion(&hadc, 100) == HAL_OK){ /* Channel 1 */
		media_1 = HAL_ADC_GetValue(&hadc);
		v_1 = 0.0008*media_1;
	}
 
	HAL_ADC_Stop(&hadc); /* stop the ADC */
	HAL_Delay(100); /* 100 ms delay before starting ADC again */
 }
}
 
void SendByte(int channel){
 
	Output_Linha = channel;
	for (i = 0; i < 8; i++) {
		if (Output_Linha & (1 << i)) {
			HAL_GPIO_WritePin(GPIOC, GPIO_PIN_12, GPIO_PIN_RESET); 
		} else {
			HAL_GPIO_WritePin(GPIOC, GPIO_PIN_12, GPIO_PIN_SET); 
		}
 
		HAL_GPIO_WritePin(GPIOC, GPIO_PIN_10, GPIO_PIN_SET);
		HAL_Delay(50);
		HAL_GPIO_WritePin(GPIOC, GPIO_PIN_10, GPIO_PIN_RESET); 
	}
 
	HAL_GPIO_WritePin(GPIOC, GPIO_PIN_11, GPIO_PIN_SET); 
	HAL_Delay(50);
	HAL_GPIO_WritePin(GPIOC, GPIO_PIN_11, GPIO_PIN_RESET); 
 
}

The configuration of the ADC is as it follows:

static void MX_ADC_Init(void)
{
 
 ADC_ChannelConfTypeDef sConfig = {0};
 
 hadc.Instance = ADC1;
 hadc.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1;
 hadc.Init.Resolution = ADC_RESOLUTION_12B;
 hadc.Init.DataAlign = ADC_DATAALIGN_RIGHT;
 hadc.Init.ScanConvMode = ADC_SCAN_DIRECTION_FORWARD;
 hadc.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
 hadc.Init.LowPowerAutoWait = DISABLE;
 hadc.Init.LowPowerAutoPowerOff = DISABLE;
 hadc.Init.ContinuousConvMode = ENABLE;
 hadc.Init.DiscontinuousConvMode = DISABLE;
 hadc.Init.ExternalTrigConv = ADC_SOFTWARE_START;
 hadc.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
 hadc.Init.DMAContinuousRequests = DISABLE;
 hadc.Init.Overrun = ADC_OVR_DATA_OVERWRITTEN;
 if (HAL_ADC_Init(&hadc) != HAL_OK)
 {
 Error_Handler();
 }
 sConfig.Channel = ADC_CHANNEL_0;
 sConfig.Rank = ADC_RANK_CHANNEL_NUMBER;
 sConfig.SamplingTime = ADC_SAMPLETIME_1CYCLE_5;
 if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 
 sConfig.Channel = ADC_CHANNEL_1;
 if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
}

 I used CubeMX to generate the code. If you think you need something else to help me, please ask.

This topic has been closed for replies.

1 reply

waclawek.jan
Super User
Jun 10, 2019 7:20 PM UTC

I don't use nor understand Cube, but if you poll for the ADC result, don't use Continuous mode, and convert only one channel at a time, reconfigure ADC for the other channel, and start it again.

JW