Skip to main content
Shruthi
Associate III
Feb 21, 2021 6:00 PM UTC
Question

I am using STM32F746G-discovery kit with 6.1.1 CubeMX version and updated firmware. I have created a cubeMX default project and tried to build it. Build is successful but when I try to run that on the development kit, it does not download successfull

Info : STM32F746NGHx.cpu: hardware has 8 breakpoints, 4 watchpoints

Info : Listening on port 3333 for gdb connections

target halted due to debug-request, current mode: Thread 

xPSR: 0x01000000 pc: 0x0800b664 msp: 0x20050000

Info : Stlink adapter speed set to 1800 kHz

adapter speed: 1800 kHz

** Programming Started **

auto erase enabled

Info : flash size probed value 1024

target halted due to breakpoint, current mode: Thread 

xPSR: 0x61000000 pc: 0x20000084 msp: 0x20050000

wrote 65536 bytes from file Debug/PeripheralsTrial.elf in 1.273580s (50.252 KiB/s)

** Programming Finished **

** Verify Started **

target halted due to breakpoint, current mode: Thread 

xPSR: 0x61000000 pc: 0x2000002e msp: 0x20050000

verified 47680 bytes in 0.160581s (289.963 KiB/s)

** Verified OK **

** Resetting Target **

shutdown command invoked

I see that there are 8 breakpoints and 4 watchpoints in stmWorkbench. But I did not find which part of the project has this. I have also tried selecting option of 'remove all breakpoints in project' But still this error persists. Please help me with this. Im unable to start any project.

This topic has been closed for replies.