Skip to main content
VTodm.1
Associate II
May 21, 2021 3:46 PM UTC
Solved

I am trying to Pin lock a STm32H755 and i am facing partly disabled while using USB_OTG_HS in device only mode and ADC ?

The ADC in stm32cubemx will throw a warning in All three ADC's while using a USB_OTG_HS. No matter what i try the error won't go away? Has anyone experienced this?? Will it cause any trouble in functioning of ADC?

This topic has been closed for replies.
TDK
TDKBest answer
May 21, 2021 3:50 PM UTC

Hover over the iron to find out the issue. Likely it's just saying that ADC channel cannot be enabled because those pins are in use by the USB, which is not a problem.

"If you feel a post has answered your question, please click ""Accept as Solution""."

2 replies

TDK
TDKBest answer
May 21, 2021 3:50 PM UTC

Hover over the iron to find out the issue. Likely it's just saying that ADC channel cannot be enabled because those pins are in use by the USB, which is not a problem.

"If you feel a post has answered your question, please click ""Accept as Solution""."
VTodm.1
VTodm.1Author
Associate II
May 21, 2021 5:25 PM UTC

It just says Partly disabled due to USB_HS in Device only mode and some of the pins are disabled ! i m just concerned it won't create any problems with the working of ADC on other pins which are available ! i just wanna confirm it ! Thank you