Skip to main content
Explorer
April 1, 2026
Solved

HRTIM configuration when updated to 6.16.1 CubeMX

  • April 1, 2026
  • 1 reply
  • 344 views

Hi,

In STM32CubeIDE/MX versions 1.19 and 6.15, I configured HRTIM, and it worked fine without any errors in CubeMX. I have updated STM32CubeIDE/MX to versions 2.1.1 and 6.16.1, and I have noticed the error messages shown in the pictures below.

The dead time is not used, but when set Output 2 state MX displays the message "Set Sources: nothing to set as Dead Time is enabled, Output2 signal is defined based on Output1 Configuration Set Sources". The project operates like before the update, but it is not possible to add new Set Sources (I can only change the number of Set Sources to zero). 

How to understand this behaviour?

Krzysztof

 

 

Pic1.jpgPic2.jpg

Best answer by Ghofrane GSOURI

Hello @kkolek 

Thank you for posting.

This issue has already been detected and escalated to dev team under internal ticket ID 222461 and it will be fixed as soon as possible. 

THX

Ghofrane

1 reply

Ghofrane GSOURI
Ghofrane GSOURIBest answer
ST Technical Moderator
April 2, 2026

Hello @kkolek 

Thank you for posting.

This issue has already been detected and escalated to dev team under internal ticket ID 222461 and it will be fixed as soon as possible. 

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.