Skip to main content
aotuz
Associate
Feb 2, 2020 4:09 PM UTC
Question

How to use cubeMX created semaphores inside another source file? CubeMX creates semaphores inside app_freertos.c but they are not accessible from custom source files??

I am using STM32CubeMX with FreeRTOS/ CMSIS_RTOS_V2. However I think I have not understood the logic behind the creation of the files.

  • CubeMX created a file "app_freertos.c" without a header file and the semaphore created is inside this file.
  • I have two other files "busA.h" and "busA.c" where I use a couple of Timer ISRs with STM Low Layer APIs. "busA.h" is included inside "stm32g0xx_it.c".

I need to call osSemaphoreRelease(semaphoreId) inside one of those ISR callbacks but because CubeMX created the semaphore inside "app_freertos.c", I just can't access it. It seems the semaphore scope is limited to "app_freertos.c". The problem is I have a lot going on inside my files (busA.c), bunch of variables etc. I am %90 sure if I try to move everything inside "app_freertos.c", it will be a mess.

Shall I create a header file manually for "app_freertos.c", namely "app_freertos.h" and return semaphore address into my "busA.c" file (with a function)?

This topic has been closed for replies.

5 replies

KnarfB
Super User
Feb 2, 2020 6:39 PM UTC

I would add a header file and simply declare the semaphores like

extern osSemaphoreId_t semaphoreId;

aotuz
aotuzAuthor
Associate
Feb 2, 2020 6:58 PM UTC

cubeMX will probably create a new semaphore at the same place each time I generate code, and won't that extern limit encapsulation?

Piranha
Principal III
Feb 2, 2020 7:08 PM UTC

The real limiting factor is CubeMX - it limits sanity and stability of firmware to a level of non-working bloatware.

Piranha
Principal III
Feb 2, 2020 6:40 PM UTC

Either export higher level ISR to a global scope and call it from "***_it.c" file or put "IRQHandler" in a file with the semaphore.